InspectionSphereFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionSphereFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM inspection sphere feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionSphereFeatureBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
CenterPointX | Returns or sets the sphere center point X coordinate |
CenterPointY | Returns or sets the sphere center point Y coordinate |
CenterPointZ | Returns or sets the sphere center point Z coordinate |
ChannelName | Returns or sets the channel’s name |
CsysRefType | Returns or sets the csys ref type |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
Diameter | Returns or sets the sphere diameter |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
InnerOuterType | Returns or sets the inner outer type (spherical hole or spherical boss) |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the sphere inspection feature name |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectSphere | Returns the selected sphere |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateParams | Updates sphere inspection feature characteristic parameters based on selected geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
CenterPointX¶
-
InspectionSphereFeatureBuilder.
CenterPointX
¶ Returns or sets the sphere center point X coordinate
-------------------------------------
Getter Method
Signature
CenterPointX()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPointX(centerPointX)
Parameters: centerPointX (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CenterPointY¶
-
InspectionSphereFeatureBuilder.
CenterPointY
¶ Returns or sets the sphere center point Y coordinate
-------------------------------------
Getter Method
Signature
CenterPointY()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPointY(centerPointY)
Parameters: centerPointY (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CenterPointZ¶
-
InspectionSphereFeatureBuilder.
CenterPointZ
¶ Returns or sets the sphere center point Z coordinate
-------------------------------------
Getter Method
Signature
CenterPointZ()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPointZ(centerPointZ)
Parameters: centerPointZ (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CsysRefType¶
-
InspectionSphereFeatureBuilder.
CsysRefType
¶ Returns or sets the csys ref type
-------------------------------------
Getter Method
Signature
CsysRefType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationCsysreferencetypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CsysRefType(csysRefType)
Parameters: csysRefType ( NXOpen.CAM.CamInspectionOperationCsysreferencetypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Diameter¶
-
InspectionSphereFeatureBuilder.
Diameter
¶ Returns or sets the sphere diameter
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: float New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter(diameter)
Parameters: diameter (float) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
InnerOuterType¶
-
InspectionSphereFeatureBuilder.
InnerOuterType
¶ Returns or sets the inner outer type (spherical hole or spherical boss)
-------------------------------------
Getter Method
Signature
InnerOuterType()
Returns: Return type: NXOpen.CAM.CamInspectionOperationInneroutertypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
InnerOuterType(innerOuterType)
Parameters: innerOuterType ( NXOpen.CAM.CamInspectionOperationInneroutertypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionSphereFeatureBuilder.
Name
¶ Returns or sets the sphere inspection feature name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectSphere¶
-
InspectionSphereFeatureBuilder.
SelectSphere
¶ Returns the selected sphere
-------------------------------------
Getter Method
Signature
SelectSphere()
Returns: Return type: NXOpen.SelectNXObject
New in version NX7.0.0.
License requirements: None.
Method Detail¶
UpdateParams¶
-
InspectionSphereFeatureBuilder.
UpdateParams
¶ Updates sphere inspection feature characteristic parameters based on selected geometry
Signature
UpdateParams()
New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionSphereFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.