InspectionProbeTipTypeBuilder Class¶
-
class
NXOpen.CAM.
InspectionProbeTipTypeBuilder
¶ Bases:
NXOpen.CAM.InheritableBuilder
Represents a builder for an inheritable probe tip type value
New in version NX9.0.1.
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the preferred probe tip type |
Methods¶
Property Detail¶
Value¶
-
InspectionProbeTipTypeBuilder.
Value
¶ Returns or sets the preferred probe tip type
-------------------------------------
Getter Method
Signature
Value()
Returns: the current preferred probe tip type Return type: NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value(itemValue)
Parameters: itemValue ( NXOpen.CAM.InspectionMoveBuilderProbeTipTypes
) – the new preferred probe tip typeNew in version NX9.0.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)