InheritableFeedModeBuilder Class

class NXOpen.CAM.InheritableFeedModeBuilder

Bases: NXOpen.CAM.InheritableBuilder

Represents a builder for an inheritable enum value in of a CAM.

CAMObject .. versionadded:: NX8.0.0

Properties

Property Description
InheritanceStatus Returns or sets the inheritance status
Tag Returns the Tag for this object.
Value Returns or sets the current value

Methods

Property Detail

Value

InheritableFeedModeBuilder.Value

Returns or sets the current value

-------------------------------------

Getter Method

Signature Value()

Returns:the current value
Return type:NXOpen.CAM.FeedRapidOutputMode

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Value(itemValue)

Parameters:itemValue (NXOpen.CAM.FeedRapidOutputMode) – the new value

New in version NX8.0.0.

License requirements: cam_base (“CAM BASE”)