FeedRapidOutputMode Enumeration

class NXOpen.CAM.FeedRapidOutputMode

Bases: object

The type for rapid feed output mode

New in version NX8.0.0.

Enum Members

Enum Member Enum Member Description
G0
G0–non interpolated rapid motion
G1
G1–interpolated motion
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.