DrillMethodBuilder Class¶
-
class
NXOpen.CAM.
DrillMethodBuilder
¶ Bases:
NXOpen.CAM.MethodBuilder
Represents a Drill Method Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateDrillMethodBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
CutParameters | Returns the cut parameter object |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds builder |
OptimizationMethod | Returns or sets the optim method |
PaintDisplay | Returns the sub builder for paint display |
PathDisplay | Returns the sub builder for path display |
PathDisplayColors | Returns the sub builder for path display colors |
SilhouDisplay | Returns the sub builder for silhou display |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolDisplay | Returns the sub builder for tool display |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCutMethod | Get cut method @return |
GetObject | Returns the object currently being edited by this builder. |
SetCutMethod | Set cut method |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
FeedsBuilder¶
-
DrillMethodBuilder.
FeedsBuilder
¶ Returns the feeds builder
-------------------------------------
Getter Method
Signature
FeedsBuilder()
Returns: the feeds builder Return type: NXOpen.CAM.FeedsBuilder
New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
DrillMethodBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.