ResponseResultsEvaluationSettingBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
ResponseResultsEvaluationSettingBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.DynamicResultEvaluationSettingBuilder
This is a manager to the
NXOpen.CAE.ResponseSimulation.ResponseResultsEvaluationSetting
class.Object of type
NXOpen.CAE.ResponseSimulation.ResponseResultsEvaluationSetting
can be created and edited only through this classTo create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.EvaluationSettingManager.CreateResponseResultsEvaluationSettingBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
DecimationOrder | Returns or sets the decimation order of domain setting. |
EndPoint | Returns or sets the end value of domain setting. |
PointValue | Returns or sets the method choosed to define select point value. |
ResponseDomainDefinitionOption | Returns or sets the method choosed to define response domain |
StartPoint | Returns or sets the start value of domain setting. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDescriptionString | Returns the description. |
GetDestinationElements | Returns the destination elements @return |
GetDestinationNodes | Returns the destination nodes @return |
GetObject | Returns the object currently being edited by this builder. |
GetOutputOptions | Returns the output options @return |
GetPointsValueList | Returns the points value list @return |
SetDescriptionString | Sets the description |
SetDestinationElements | Sets the destination elements |
SetDestinationNodes | Sets the destination nodes |
SetOutputOptions | Sets the output options |
SetPointsValueList | Sets the points value list |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
DecimationOrder¶
-
ResponseResultsEvaluationSettingBuilder.
DecimationOrder
¶ Returns or sets the decimation order of domain setting.
Only available when response domain is
CAE.ResponseSimulationResponseDomainDefinitionMethod.StartEndPoint
-------------------------------------
Getter Method
Signature
DecimationOrder()
Returns: Return type: int New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
DecimationOrder(decimationOrder)
Parameters: decimationOrder (int) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
EndPoint¶
-
ResponseResultsEvaluationSettingBuilder.
EndPoint
¶ Returns or sets the end value of domain setting.
Only available when response domain is
CAE.ResponseSimulationResponseDomainDefinitionMethod.StartEndPoint
-------------------------------------
Getter Method
Signature
EndPoint()
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
EndPoint(endPoint)
Parameters: endPoint (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
PointValue¶
-
ResponseResultsEvaluationSettingBuilder.
PointValue
¶ Returns or sets the method choosed to define select point value.
Only available when response domain is
CAE.ResponseSimulationResponseDomainDefinitionMethod.KeyIn
-------------------------------------
Getter Method
Signature
PointValue()
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
PointValue(pointValue)
Parameters: pointValue (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ResponseDomainDefinitionOption¶
-
ResponseResultsEvaluationSettingBuilder.
ResponseDomainDefinitionOption
¶ Returns or sets the method choosed to define response domain
-------------------------------------
Getter Method
Signature
ResponseDomainDefinitionOption()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ResponseDomainDefinitionMethod
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ResponseDomainDefinitionOption(definitionMethod)
Parameters: definitionMethod ( NXOpen.CAE.ResponseSimulation.ResponseDomainDefinitionMethod
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
StartPoint¶
-
ResponseResultsEvaluationSettingBuilder.
StartPoint
¶ Returns or sets the start value of domain setting.
Only available when response domain is
CAE.ResponseSimulationResponseDomainDefinitionMethod.StartEndPoint
-------------------------------------
Getter Method
Signature
StartPoint()
Returns: Return type: float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
StartPoint(startPoint)
Parameters: startPoint (float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
GetDestinationElements¶
-
ResponseResultsEvaluationSettingBuilder.
GetDestinationElements
¶ Returns the destination elements
Signature
GetDestinationElements()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetDestinationNodes¶
-
ResponseResultsEvaluationSettingBuilder.
GetDestinationNodes
¶ Returns the destination nodes
Signature
GetDestinationNodes()
Returns: Return type: list of NXOpen.CAE.FENode
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetOutputOptions¶
-
ResponseResultsEvaluationSettingBuilder.
GetOutputOptions
¶ Returns the output options
Signature
GetOutputOptions()
Returns: Return type: list of NXOpen.CAE.ResponseSimulation.EvaluationResultType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
GetPointsValueList¶
-
ResponseResultsEvaluationSettingBuilder.
GetPointsValueList
¶ Returns the points value list
Signature
GetPointsValueList()
Returns: Return type: list of float New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetDestinationElements¶
-
ResponseResultsEvaluationSettingBuilder.
SetDestinationElements
¶ Sets the destination elements
Signature
SetDestinationElements(destinationElement)
Parameters: destinationElement (list of NXOpen.CAE.FEElement
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetDestinationNodes¶
-
ResponseResultsEvaluationSettingBuilder.
SetDestinationNodes
¶ Sets the destination nodes
Signature
SetDestinationNodes(destinationNodes)
Parameters: destinationNodes (list of NXOpen.CAE.FENode
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetOutputOptions¶
-
ResponseResultsEvaluationSettingBuilder.
SetOutputOptions
¶ Sets the output options
Signature
SetOutputOptions(outputOptions)
Parameters: outputOptions (list of NXOpen.CAE.ResponseSimulation.EvaluationResultType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
SetPointsValueList¶
-
ResponseResultsEvaluationSettingBuilder.
SetPointsValueList
¶ Sets the points value list
Signature
SetPointsValueList(pointsValueList)
Parameters: pointsValueList (list of float) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Validate¶
-
ResponseResultsEvaluationSettingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.