PrlResultsEvaluationSettingBuilder Class

class NXOpen.CAE.ResponseSimulation.PrlResultsEvaluationSettingBuilder

Bases: NXOpen.CAE.ResponseSimulation.DynamicResultEvaluationSettingBuilder

Represents the abstract builder class of evaluation setting for peak value, RMS results and LCR results.

This is an abstract class, and cannot be created.

New in version NX5.0.0.

Properties

Property Description
CoordinateSystem Returns or sets the coordinate system.
ObservationNode Returns or sets the relative node.
Relative Returns or sets the option of using the observation node in evaluation
ResultType Returns or sets the result type
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetDataComponents Returns the direction data components.
GetDescriptionString Returns the description.
GetObject Returns the object currently being edited by this builder.
GetOutputElements Returns the destination elements.
GetOutputNodes Returns the destination nodes.
SetDataComponents Sets the direction data components.
SetDescriptionString Sets the description
SetOutputElements Sets the destination elements
SetOutputNodes Sets the destination nodes
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

CoordinateSystem

PrlResultsEvaluationSettingBuilder.CoordinateSystem

Returns or sets the coordinate system.

Only available when the result type is NXOpen.CAE.ResponseSimulation.EvaluationResultType.Stress, NXOpen.CAE.ResponseSimulation.EvaluationResultType.ShellResultant

-------------------------------------

Getter Method

Signature CoordinateSystem()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.CoordinateSystem

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature CoordinateSystem(coordinateSystem)

Parameters:coordinateSystem (NXOpen.CAE.ResponseSimulation.CoordinateSystem) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ObservationNode

PrlResultsEvaluationSettingBuilder.ObservationNode

Returns or sets the relative node.

Only available when result type is NXOpen.CAE.ResponseSimulation.EvaluationResultType.Displacement, NXOpen.CAE.ResponseSimulation.EvaluationResultType.Acceleration, NXOpen.CAE.ResponseSimulation.EvaluationResultType.ElementForce

-------------------------------------

Getter Method

Signature ObservationNode()

Returns:
Return type:NXOpen.CAE.FENode

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature ObservationNode(relativeNode)

Parameters:relativeNode (NXOpen.CAE.FENode) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Relative

PrlResultsEvaluationSettingBuilder.Relative

Returns or sets the option of using the observation node in evaluation

-------------------------------------

Getter Method

Signature Relative()

Returns:
Return type:bool

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature Relative(relative)

Parameters:relative (bool) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ResultType

PrlResultsEvaluationSettingBuilder.ResultType

Returns or sets the result type

-------------------------------------

Getter Method

Signature ResultType()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.EvaluationResultType

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

-------------------------------------

Setter Method

Signature ResultType(resultType)

Parameters:resultType (NXOpen.CAE.ResponseSimulation.EvaluationResultType) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

GetDataComponents

PrlResultsEvaluationSettingBuilder.GetDataComponents

Returns the direction data components.

The condidate choices will be changed according to NXOpen.CAE.ResponseSimulation.EvaluationResultType setting

Signature GetDataComponents()

Returns:
Return type:list of NXOpen.CAE.ResponseSimulation.DirectionDataComponent

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

GetOutputElements

PrlResultsEvaluationSettingBuilder.GetOutputElements

Returns the destination elements.

Only available when the result type is NXOpen.CAE.ResponseSimulation.EvaluationResultType.Stress, NXOpen.CAE.ResponseSimulation.EvaluationResultType.ShellResultant

Signature GetOutputElements()

Returns:
Return type:list of NXOpen.CAE.FEElement

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

GetOutputNodes

PrlResultsEvaluationSettingBuilder.GetOutputNodes

Returns the destination nodes.

Only available when result type is NXOpen.CAE.ResponseSimulation.EvaluationResultType.Displacement, NXOpen.CAE.ResponseSimulation.EvaluationResultType.Acceleration, NXOpen.CAE.ResponseSimulation.EvaluationResultType.ElementForce

Signature GetOutputNodes()

Returns:
Return type:list of NXOpen.CAE.FENode

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SetDataComponents

PrlResultsEvaluationSettingBuilder.SetDataComponents

Sets the direction data components.

The condidate choices will be changed according to NXOpen.CAE.ResponseSimulation.EvaluationResultType setting

Signature SetDataComponents(dataComponent)

Parameters:dataComponent (list of NXOpen.CAE.ResponseSimulation.DirectionDataComponent) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SetOutputElements

PrlResultsEvaluationSettingBuilder.SetOutputElements

Sets the destination elements

Signature SetOutputElements(destinationElements)

Parameters:destinationElements (list of NXOpen.CAE.FEElement) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

SetOutputNodes

PrlResultsEvaluationSettingBuilder.SetOutputNodes

Sets the destination nodes

Signature SetOutputNodes(destinationNodes)

Parameters:destinationNodes (list of NXOpen.CAE.FENode) –

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Validate

PrlResultsEvaluationSettingBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.