ExcitationBuilder Class

class NXOpen.CAE.ResponseSimulation.ExcitationBuilder

Bases: NXOpen.CAE.ResponseSimulation.BaseBuilder

Represents the abstract excitation builder class.

Any of real excitation builder must inherit from this class.

This is an abstract class, and cannot be created.

New in version NX5.0.0.

Properties

Property Description
DynamicEvent Returns the parent dynamic event object
ExcitationLocationDefinition Returns the excitation location definition
ObjectLabel Returns the object label
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

ExcitationBuilderExcitationLocationType Enumeration the type of excitation location

Property Detail

DynamicEvent

ExcitationBuilder.DynamicEvent

Returns the parent dynamic event object

-------------------------------------

Getter Method

Signature DynamicEvent()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.RSEvent

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

ExcitationLocationDefinition

ExcitationBuilder.ExcitationLocationDefinition

Returns the excitation location definition

-------------------------------------

Getter Method

Signature ExcitationLocationDefinition()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.ExcitationLocationDefinition

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

Validate

ExcitationBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.