ExcitationLocationDefinition Class¶
-
class
NXOpen.CAE.ResponseSimulation.
ExcitationLocationDefinition
¶ Bases:
NXOpen.TaggedObject
Represents the manager to
CAE.ResponseSimulation.DistributedLoadExcitation
.The object of type
CAE.ResponseSimulation.DistributedLoadExcitation
can only be created or edited through this class.New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ExcitationLocation | Returns the excitation location on which the excitation will be applied. |
ExcitationLocationId | Returns or sets the ID of excitation location on which the excitation will be applied. |
ExcitationLocationType | Returns or sets the type of excitaion location |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
ExcitationLocation¶
-
ExcitationLocationDefinition.
ExcitationLocation
¶ Returns the excitation location on which the excitation will be applied.
The excitation location type could be force location, enforced motion location or dynamic load defined in response dynamic solution
-------------------------------------
Getter Method
Signature
ExcitationLocation()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ExcitationLocationId¶
-
ExcitationLocationDefinition.
ExcitationLocationId
¶ Returns or sets the ID of excitation location on which the excitation will be applied.
The excitation location ID could be node label or load set label
-------------------------------------
Getter Method
Signature
ExcitationLocationId()
Returns: Return type: int New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ExcitationLocationId(excitaitonLocationId)
Parameters: excitaitonLocationId (int) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ExcitationLocationType¶
-
ExcitationLocationDefinition.
ExcitationLocationType
¶ Returns or sets the type of excitaion location
-------------------------------------
Getter Method
Signature
ExcitationLocationType()
Returns: Return type: NXOpen.CAE.ResponseSimulation.ExcitationBuilderExcitationLocationType
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ExcitationLocationType(excitationLocationType)
Parameters: excitationLocationType ( NXOpen.CAE.ResponseSimulation.ExcitationBuilderExcitationLocationType
) –New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)