BaseBuilder Class

class NXOpen.CAE.ResponseSimulation.BaseBuilder

Bases: NXOpen.Builder

Represents the abstract builder class for all objects defined in response analysis meta solution

This is an abstract class, and cannot be created.

New in version NX5.0.0.

Properties

Property Description
ObjectLabel Returns the object label
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

ObjectLabel

BaseBuilder.ObjectLabel

Returns the object label

-------------------------------------

Getter Method

Signature ObjectLabel()

Returns:
Return type:NXOpen.CAE.ResponseSimulation.ObjectLabel

New in version NX5.0.0.

License requirements: nx_response_anlys (“NX Response Analysis”)

Method Detail

Validate

BaseBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.