TBSConstraintBuilder Class¶
-
class
NXOpen.CAE.Optimization.
TBSConstraintBuilder
¶ Bases:
NXOpen.Builder
Represents the builder of
NXOpen.CAE.Optimization.TBSConstraint
To create a new instance of this class, use
NXOpen.CAE.Optimization.TBSOptimizationManager.CreateResponseConstraintBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
ConstraintType | Returns or sets the constraint type |
ConstraintValue | Returns the constrain value |
DesignResponse | Returns or sets the design response |
Magnitude | Returns or sets the magnitude type of the constraint |
NameDescription | Returns the name description |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TBSConstraintBuilderConstraintOption Enumeration | Defines the constraint type |
TBSConstraintBuilderMagnitudeType Enumeration | Defines the type of constraint value |
Property Detail¶
ConstraintType¶
-
TBSConstraintBuilder.
ConstraintType
¶ Returns or sets the constraint type
-------------------------------------
Getter Method
Signature
ConstraintType()
Returns: Return type: NXOpen.CAE.Optimization.TBSConstraintBuilderConstraintOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ConstraintType(constraintType)
Parameters: constraintType ( NXOpen.CAE.Optimization.TBSConstraintBuilderConstraintOption
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
ConstraintValue¶
-
TBSConstraintBuilder.
ConstraintValue
¶ Returns the constrain value
-------------------------------------
Getter Method
Signature
ConstraintValue()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
DesignResponse¶
-
TBSConstraintBuilder.
DesignResponse
¶ Returns or sets the design response
-------------------------------------
Getter Method
Signature
DesignResponse()
Returns: Return type: NXOpen.CAE.Optimization.TBSDesignResponse
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DesignResponse(designResponse)
Parameters: designResponse ( NXOpen.CAE.Optimization.TBSDesignResponse
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Magnitude¶
-
TBSConstraintBuilder.
Magnitude
¶ Returns or sets the magnitude type of the constraint
-------------------------------------
Getter Method
Signature
Magnitude()
Returns: Return type: NXOpen.CAE.Optimization.TBSConstraintBuilderMagnitudeType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Magnitude(magnitude)
Parameters: magnitude ( NXOpen.CAE.Optimization.TBSConstraintBuilderMagnitudeType
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
NameDescription¶
-
TBSConstraintBuilder.
NameDescription
¶ Returns the name description
-------------------------------------
Getter Method
Signature
NameDescription()
Returns: Return type: NXOpen.CAE.Optimization.NameDescription
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TBSConstraintBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.