TBSConstraintBuilderMagnitudeType Enumeration¶
NXOpen.CAE.Optimization.TBSConstraintBuilder.MagnitudeType is an alias for NXOpen.CAE.Optimization.TBSConstraintBuilderMagnitudeType
-
class
NXOpen.CAE.Optimization.
TBSConstraintBuilderMagnitudeType
¶ Bases:
object
Defines the type of constraint value
Enum Members
Enum Member Enum Member Description Relative Constraints could be given in relative valuesAbsolute Constraints could be given in absolute values-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-