TBSConstraintBuilderConstraintOption Enumeration¶
NXOpen.CAE.Optimization.TBSConstraintBuilder.ConstraintOption is an alias for NXOpen.CAE.Optimization.TBSConstraintBuilderConstraintOption
-
class
NXOpen.CAE.Optimization.
TBSConstraintBuilderConstraintOption
¶ Bases:
object
Defines the constraint type
Enum Members
Enum Member Enum Member Description Eq Value of equality constraintLt Value of greater or equal constraintGt Value of less or equal constraint-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-