ElementMaterialOrientationCheckBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
ElementMaterialOrientationCheckBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder
used to check the material orientation for shell and solid elements.Use
Builder.Commit()
to calculate material orientation and to display an orientation vector for each input element. UseNXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder.DoCheck()
to calculate the material orientation for each input element and return the orientation vector result. If an element fails when calculating it’s material orientation, the element will be displayed in red and outputed to listing information window.To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateElementMaterialOrientationCheckBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
SelectionList | Returns the selected objects to be checked. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DoCheck | Calculates material orientation vector for input elements and returns the orientation vector result @return material orientation vector |
GetCheckOrientation | Gets option value which indicates whether to check for the specified material orientation type @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetOrientationColor | Gets display color of a specified material orientation type @return |
SetCheckOrientation | Sets option value which indicates whether to check for the specified material orientation type |
SetOrientationColor | Sets display color of a specified material orientation type |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementMaterialOrientationCheckBuilderMaterialOrientationType Enumeration | the material orientation type |
Property Detail¶
SelectionList¶
-
ElementMaterialOrientationCheckBuilder.
SelectionList
¶ Returns the selected objects to be checked.
The objects must be
NXOpen.CAE.Mesh
orNXOpen.CAE.FEElement
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
DoCheck¶
-
ElementMaterialOrientationCheckBuilder.
DoCheck
¶ Calculates material orientation vector for input elements and returns the orientation vector result
Signature
DoCheck()
Returns: a tuple Return type: A tuple consisting of (orienation, orientationType, elements). orienation is a list of NXOpen.Vector3d
. material orientation vector orientationType is a list ofNXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilderMaterialOrientationType
. elements is a list ofNXOpen.CAE.FEElement
. the elements associated with the orientation vectorsNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GetCheckOrientation¶
-
ElementMaterialOrientationCheckBuilder.
GetCheckOrientation
¶ Gets option value which indicates whether to check for the specified material orientation type
Signature
GetCheckOrientation(orientationType)
Parameters: orientationType ( NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilderMaterialOrientationType
) –Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
GetOrientationColor¶
-
ElementMaterialOrientationCheckBuilder.
GetOrientationColor
¶ Gets display color of a specified material orientation type
Signature
GetOrientationColor(orientationType)
Parameters: orientationType ( NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilderMaterialOrientationType
) –Returns: Return type: Id New in version NX8.5.0.
License requirements: None.
SetCheckOrientation¶
-
ElementMaterialOrientationCheckBuilder.
SetCheckOrientation
¶ Sets option value which indicates whether to check for the specified material orientation type
Signature
SetCheckOrientation(orientationType, checkOrientation)
Parameters: - orientationType (
NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilderMaterialOrientationType
) – - checkOrientation (bool) –
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- orientationType (
SetOrientationColor¶
-
ElementMaterialOrientationCheckBuilder.
SetOrientationColor
¶ Sets display color of a specified material orientation type
Signature
SetOrientationColor(orientationType, color)
Parameters: - orientationType (
NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilderMaterialOrientationType
) – - color (Id) –
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
- orientationType (
Validate¶
-
ElementMaterialOrientationCheckBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.