ElementMaterialOrientationCheckBuilderMaterialOrientationType Enumeration¶
NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilder.MaterialOrientationType is an alias for NXOpen.CAE.ModelCheck.ElementMaterialOrientationCheckBuilderMaterialOrientationType
-
class
NXOpen.CAE.ModelCheck.
ElementMaterialOrientationCheckBuilderMaterialOrientationType
¶ Bases:
object
the material orientation type
Enum Members
Enum Member Enum Member Description Shell the material orientation of shell elementSolidFirstDirection the first direction of solid element material orientationSolidSecondDirection the second direction of solid element material orientationSolidThirdDirection the third direction of solid element material orientation-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-