ElementEdgeCheckBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
ElementEdgeCheckBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder
which can be used to detect free element edges or non-manifold edges.A free edge is any Element edge that is not shared by any other element face (on either 2D or 3D elements ) within the defined scope of the check. A non-manifold edge is any Element edge that is shared more than 2 element faces (on either 2D or 3D elements ) within the defined scope of the check.
The computation scope
ElementEdgeCheckBuilder.ComputationScope`()
will affect on the checking result. The free element edges or non-manifold edges found will be displayed using the display settingNXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderEdgeDisplayStyle_Struct
. You can execute checking throughBuilder.Commit()
orNXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder.ExecuteCheck()
. Commiting the builder performs checking and displays the free edges and non-manifold edges in graphic window.To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateElementEdgeCheckBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
CheckFreeEdges | Returns or sets the value indicating whether to check free edges or not |
CheckNonManifoldEdges | Returns or sets the value indicating whether to check non-manifold edges or not |
ComputationScope | Returns or sets the computation scope |
FreeEdgeDisplayStyle | Returns or sets the display style for free edges detected |
NonManifoldEdgeDisplayStyle | Returns or sets the displaying style for non-manifold edges detected |
SelectionList | Returns the selected objects to be checked. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DoCheck | Finds free edges when CAE.ModelCheck.ElementEdgeCheckBuilder.CheckFreeEdges`() is set, and non-manifold edges when CAE.ModelCheck.ElementEdgeCheckBuilder.CheckNonManifoldEdges`() is set, returns the associated elements and output group for free and/or non-manifold element edges. |
ExecuteCheck | Finds free edges when CAE.ModelCheck.ElementEdgeCheckBuilder.CheckFreeEdges`() is set, and non-manifold edges when CAE.ModelCheck.ElementEdgeCheckBuilder.CheckNonManifoldEdges`() is set. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
HideInputMeshes | Hides or unhides the input meshes |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ElementEdgeCheckBuilderScope Enumeration | the Scope over which the Computation of free/non-manifold edges with be done |
Structs¶
ElementEdgeCheckBuilderEdgeDisplayStyle_Struct Struct | the display style of the edges detected |
Property Detail¶
CheckFreeEdges¶
-
ElementEdgeCheckBuilder.
CheckFreeEdges
¶ Returns or sets the value indicating whether to check free edges or not
-------------------------------------
Getter Method
Signature
CheckFreeEdges()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckFreeEdges(checkFreeEdges)
Parameters: checkFreeEdges (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
CheckNonManifoldEdges¶
-
ElementEdgeCheckBuilder.
CheckNonManifoldEdges
¶ Returns or sets the value indicating whether to check non-manifold edges or not
-------------------------------------
Getter Method
Signature
CheckNonManifoldEdges()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckNonManifoldEdges(checkNonManifoldEdges)
Parameters: checkNonManifoldEdges (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ComputationScope¶
-
ElementEdgeCheckBuilder.
ComputationScope
¶ Returns or sets the computation scope
-------------------------------------
Getter Method
Signature
ComputationScope()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderScope
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComputationScope(computationScope)
Parameters: computationScope ( NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderScope
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FreeEdgeDisplayStyle¶
-
ElementEdgeCheckBuilder.
FreeEdgeDisplayStyle
¶ Returns or sets the display style for free edges detected
-------------------------------------
Getter Method
Signature
FreeEdgeDisplayStyle()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderEdgeDisplayStyle_Struct
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FreeEdgeDisplayStyle(freeEdgesStyle)
Parameters: freeEdgesStyle ( NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderEdgeDisplayStyle_Struct
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
NonManifoldEdgeDisplayStyle¶
-
ElementEdgeCheckBuilder.
NonManifoldEdgeDisplayStyle
¶ Returns or sets the displaying style for non-manifold edges detected
-------------------------------------
Getter Method
Signature
NonManifoldEdgeDisplayStyle()
Returns: Return type: NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderEdgeDisplayStyle_Struct
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NonManifoldEdgeDisplayStyle(nonManifoldEdgeStyle)
Parameters: nonManifoldEdgeStyle ( NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderEdgeDisplayStyle_Struct
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SelectionList¶
-
ElementEdgeCheckBuilder.
SelectionList
¶ Returns the selected objects to be checked.
The objects must be
NXOpen.CAE.Mesh
orNXOpen.CAE.FEElement
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
DoCheck¶
-
ElementEdgeCheckBuilder.
DoCheck
¶ Finds free edges when
CAE.ModelCheck.ElementEdgeCheckBuilder.CheckFreeEdges`()
is set, and non-manifold edges whenCAE.ModelCheck.ElementEdgeCheckBuilder.CheckNonManifoldEdges`()
is set, returns the associated elements and output group for free and/or non-manifold element edges.For the associated elements, if both checks are done at the same time, the elements associated to free edges are returned firstly in the list.
Signature
DoCheck()
Returns: a tuple Return type: A tuple consisting of (freeEdges, nonManifoldEdges, assoElems, outputGroup). freeEdges is a list of NXOpen.CAE.FEElemEdge
. free element edges nonManifoldEdges is a list ofNXOpen.CAE.FEElemEdge
. non-manifold element edges assoElems is a list ofNXOpen.CAE.FEElement
. associated elements for free and/or non-manifold element edges, if both checks are done at the same time, the elements associated to free edges are returned firstly in the list. outputGroup is aNXOpen.CAE.CaeGroup
. output group for free and/or non-manifold element edgesNew in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ExecuteCheck¶
-
ElementEdgeCheckBuilder.
ExecuteCheck
¶ Finds free edges when
CAE.ModelCheck.ElementEdgeCheckBuilder.CheckFreeEdges`()
is set, and non-manifold edges whenCAE.ModelCheck.ElementEdgeCheckBuilder.CheckNonManifoldEdges`()
is set.The method
Builder.Commit()
will also do the same thing, but display the element edges instead of returning them.Signature
ExecuteCheck()
Returns: a tuple Return type: A tuple consisting of (freeEdges, nonManifoldEdges). freeEdges is a list of NXOpen.CAE.FEElemEdge
. free element edges nonManifoldEdges is a list ofNXOpen.CAE.FEElemEdge
. non-manifold element edgesNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
HideInputMeshes¶
-
ElementEdgeCheckBuilder.
HideInputMeshes
¶ Hides or unhides the input meshes
Signature
HideInputMeshes(hideInputMeshes)
Parameters: hideInputMeshes (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
ElementEdgeCheckBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.