ElementEdgeCheckBuilderScope Enumeration

NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilder.Scope is an alias for NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderScope

class NXOpen.CAE.ModelCheck.ElementEdgeCheckBuilderScope

Bases: object

the Scope over which the Computation of free/non-manifold edges with be done

Enum Members

Enum Member Enum Member Description
EntireModel
Takes all elements in the model into account while computing
VisibleModel
Only takes visible elements into account while computing
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.