OptionSetting Class¶
-
class
NXOpen.CAE.FTK.
OptionSetting
¶ Bases:
object
Manager the options data for AFU Data Record
Not support KF.
New in version NX6.0.0.
Methods¶
Method | Description |
---|---|
GetHeaderFlag | Get the adding header flag when export to CSV file @return If want to add header when export to CSV file |
GetRecordOptionData | Get the record options data for an AFU Data Record |
SetHeaderFlag | Set the adding header flag when export to CSV file |
SetRecordOptionData | Set the record options data for an AFU Data Record |
Method Detail¶
GetHeaderFlag¶
-
OptionSetting.
GetHeaderFlag
¶ Get the adding header flag when export to CSV file
Signature
GetHeaderFlag()
Returns: If want to add header when export to CSV file Return type: bool New in version NX7.5.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
GetRecordOptionData¶
-
OptionSetting.
GetRecordOptionData
¶ Get the record options data for an AFU Data Record
Signature
GetRecordOptionData()
Returns: a tuple Return type: A tuple consisting of (recordName, functionType, abscissaType, xUnit, ordinateType, yUnit, yDenominatorUnit, sortValueType). recordName is a str. The name of the AFU Data Record functionType is a NXOpen.CAE.XyFunctionGeneralType
. Usage type of AFU Data Record used abscissaType is aNXOpen.CAE.AfuDataAbscissaType
. Abscissa specific data type xUnit is aNXOpen.CAE.XyFunctionUnit
. Unit Code of AFU data ordinateType is aNXOpen.CAE.AfuDataOrdinateType
. Ordinate data type yUnit is aNXOpen.CAE.XyFunctionUnit
. Ordinate Numerator Unit Code of AFU data yDenominatorUnit is aNXOpen.CAE.XyFunctionUnit
. Ordinate Denominator Unit Code of AFU data sortValueType is a bool. If want to sort value in x directionNew in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SetHeaderFlag¶
-
OptionSetting.
SetHeaderFlag
¶ Set the adding header flag when export to CSV file
Signature
SetHeaderFlag(addHeader)
Parameters: addHeader (bool) – If want to add header when export to CSV file New in version NX7.5.0.
License requirements: nx_ftk (“NX Advanced Graphing”)
SetRecordOptionData¶
-
OptionSetting.
SetRecordOptionData
¶ Set the record options data for an AFU Data Record
Signature
SetRecordOptionData(recordName, functionType, abscissaType, xUnit, ordinateType, yUnit, yDenominatorUnit, sortValueType)
Parameters: - recordName (str) – The name of the AFU Data Record
- functionType (
NXOpen.CAE.XyFunctionGeneralType
) – Usage type of AFU Data Record used - abscissaType (
NXOpen.CAE.AfuDataAbscissaType
) – Abscissa specific data type - xUnit (
NXOpen.CAE.XyFunctionUnit
) – Unit Code of AFU data - ordinateType (
NXOpen.CAE.AfuDataOrdinateType
) – Ordinate data type - yUnit (
NXOpen.CAE.XyFunctionUnit
) – Unit Code of AFU data - yDenominatorUnit (
NXOpen.CAE.XyFunctionUnit
) – Unit Code of AFU data - sortValueType (bool) – If want to sort value in x direction
New in version NX9.0.0.
License requirements: nx_ftk (“NX Advanced Graphing”)