Node Class¶
-
class
NXOpen.BlockStyler.
Node
¶ Bases:
NXOpen.TaggedObject
Represents the node created and utilized by
BlockStyler.Tree
.The node represents the single row of the tree. .. versionadded:: NX7.5.0
Properties¶
Property | Description |
---|---|
CrossSelection | Returns or sets the flag indicating whether cross section is allowed. |
DisplayIcon | Returns or sets the display icon. |
DisplayText | Returns or sets the display text of node. |
FirstChildNode | Returns the first child node. |
ForegroundColor | Returns or sets the text color of the node. |
IsExpanded | Returns the flag indicating whether the node is in expanded state |
IsInserted | Returns the flag indicating whether the node is inserted in BlockStyler.Tree |
IsSelected | Returns the flag indicating whether the node is in selected state |
NextNode | Returns the next node which might not belong to the same hierarchy. |
NextSelectedNode | Returns the next selected node in the whole tree hierarchy. |
NextSiblingNode | Returns the next node which belongs to the same hierarchy. |
ParentNode | Returns the parent node. |
PreviousNode | Returns the previous node which might not belong to the same hierarchy. |
PreviousSelectedNode | Returns the previous selected node in the whole tree hierarchy. |
PreviousSiblingNode | Returns the previous node which belongs to the same hierarchy. |
SelectedIcon | Returns or sets the selected icon. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Expand | Expands/collapses the node |
GetColumnDisplayText | Gets the column text for the given columnId. |
GetNodeData |
|
GetState | Gets the node state associated with node state icon. |
ScrollTo | Scrolls horizontally and vertically to make the specific column of node appear on the tree window. |
SetColumnDisplayText | Sets the text in the column which corresponds to given columnId. |
SetState | Sets the node state which is associated with node state icon. |
Enumerations¶
NodeDragType Enumeration | Represents the drag type |
NodeDropType Enumeration | Represents the drop type |
NodeExpandOption Enumeration | Represents the Expand/Collapse option |
NodeScroll Enumeration | Represents the scroll position to be applied on node. |
Property Detail¶
CrossSelection¶
-
Node.
CrossSelection
¶ Returns or sets the flag indicating whether cross section is allowed.
It is useful when the node contains
NXOpen.DisplayableObject
as data. If the flag is true then theNXOpen.DisplayableObject
is highlighted, else not. The default value is True-------------------------------------
Getter Method
Signature
CrossSelection()
Returns: Flag indicating whether cross selection is allowed. Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CrossSelection(crossSelection)
Parameters: crossSelection (bool) – Flag indicating whether cross selection is allowed. New in version NX7.5.0.
License requirements: None.
DisplayIcon¶
-
Node.
DisplayIcon
¶ Returns or sets the display icon.
This is normal icon positioned before the node text and is displayed when the node is in unselected state.
-------------------------------------
Getter Method
Signature
DisplayIcon()
Returns: Icon. Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayIcon(icon)
Parameters: icon (str) – Icon. New in version NX7.5.0.
License requirements: None.
DisplayText¶
-
Node.
DisplayText
¶ Returns or sets the display text of node.
This is same as 0th column text of this node. Use
BlockStyler.Node.SetColumnDisplayText()
to fetch the text of other column of the same node.-------------------------------------
Getter Method
Signature
DisplayText()
Returns: Display text Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplayText(displayTest)
Parameters: displayTest (str) – Display text New in version NX7.5.0.
License requirements: None.
FirstChildNode¶
-
Node.
FirstChildNode
¶ Returns the first child node.
Returns None if child node is not present.
-------------------------------------
Getter Method
Signature
FirstChildNode()
Returns: First child node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
ForegroundColor¶
-
Node.
ForegroundColor
¶ Returns or sets the text color of the node.
The color is applicable for whole row.
-------------------------------------
Getter Method
Signature
ForegroundColor()
Returns: Foreground color Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ForegroundColor(nodeForgroundColor)
Parameters: nodeForgroundColor (int) – Foreground color. New in version NX7.5.0.
License requirements: None.
IsExpanded¶
-
Node.
IsExpanded
¶ Returns the flag indicating whether the node is in expanded state
-------------------------------------
Getter Method
Signature
IsExpanded()
Returns: Flag indicating whether node is expanded. Return type: bool New in version NX7.5.3.
License requirements: None.
IsInserted¶
-
Node.
IsInserted
¶ Returns the flag indicating whether the node is inserted in
BlockStyler.Tree
-------------------------------------
Getter Method
Signature
IsInserted()
Returns: Flag indicating whether node is inserted. Return type: bool New in version NX7.5.0.
License requirements: None.
IsSelected¶
-
Node.
IsSelected
¶ Returns the flag indicating whether the node is in selected state
-------------------------------------
Getter Method
Signature
IsSelected()
Returns: Flag indicating whether the node is in selected state. Return type: bool New in version NX7.5.3.
License requirements: None.
NextNode¶
-
Node.
NextNode
¶ Returns the next node which might not belong to the same hierarchy.
The next node either is a sibling node or belongs to other root node. Returns None if next node is not present
-------------------------------------
Getter Method
Signature
NextNode()
Returns: Next node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
NextSelectedNode¶
-
Node.
NextSelectedNode
¶ Returns the next selected node in the whole tree hierarchy.
The node on which this method is called does not have to be selected. Returns None if none of the next nodes are selected.
-------------------------------------
Getter Method
Signature
NextSelectedNode()
Returns: Selected node following the provided node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
NextSiblingNode¶
-
Node.
NextSiblingNode
¶ Returns the next node which belongs to the same hierarchy.
Returns None null if next sibling node is not present.
-------------------------------------
Getter Method
Signature
NextSiblingNode()
Returns: Next sibling node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
ParentNode¶
-
Node.
ParentNode
¶ Returns the parent node.
Returns None if parent node is not present
-------------------------------------
Getter Method
Signature
ParentNode()
Returns: Parent node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
PreviousNode¶
-
Node.
PreviousNode
¶ Returns the previous node which might not belong to the same hierarchy.
Returns None null if previous node is not present
-------------------------------------
Getter Method
Signature
PreviousNode()
Returns: Previous node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
PreviousSelectedNode¶
-
Node.
PreviousSelectedNode
¶ Returns the previous selected node in the whole tree hierarchy.
The node on which this method is called does not have to be selected. Returns None if none of the previous nodes are selected.
-------------------------------------
Getter Method
Signature
PreviousSelectedNode()
Returns: Previous selected node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
PreviousSiblingNode¶
-
Node.
PreviousSiblingNode
¶ Returns the previous node which belongs to the same hierarchy.
Returns None if previous sibling node is not present.
-------------------------------------
Getter Method
Signature
PreviousSiblingNode()
Returns: Previous sibling node. Return type: NXOpen.BlockStyler.Node
New in version NX7.5.0.
License requirements: None.
SelectedIcon¶
-
Node.
SelectedIcon
¶ Returns or sets the selected icon.
This icon appears on node selection and is positioned before the node text replacing the
BlockStyler.Node.DisplayIcon`()
.-------------------------------------
Getter Method
Signature
SelectedIcon()
Returns: Icon Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectedIcon(icon)
Parameters: icon (str) – Icon. New in version NX7.5.0.
License requirements: None.
Method Detail¶
Expand¶
-
Node.
Expand
¶ Expands/collapses the node
Signature
Expand(expandOption)
Parameters: expandOption ( NXOpen.BlockStyler.NodeExpandOption
) – Expand optionNew in version NX7.5.0.
License requirements: None.
GetColumnDisplayText¶
-
Node.
GetColumnDisplayText
¶ Gets the column text for the given columnId.
The text is interpreted as icon if the column display type is
BlockStyler.TreeColumnDisplay.Icon
.Signature
GetColumnDisplayText(columnID)
Parameters: columnID (int) – Unique column id of the column. Returns: Text associated with column. Return type: str New in version NX7.5.0.
License requirements: None.
GetNodeData¶
-
Node.
GetNodeData
¶ Gets node data which contains the data in the form of unique name-value pairs. In this context unique name is termed as property name. There could me more than one such property name - value pair, but the property name of the primary data should be named “Data” (case-sensitive). For instance, if a
BlockStyler.Node
represents a feature object then property name should be “Data” and the value should be feature object. The primary data is used by NX for some operations such cross selection.Initialy the container or list is empty and it is expected that data would be added to it. Additional property name - value pair can be added to the container or list, but it should be made sure that there is no dublicate property name exists in the container or list. The additional data can be seen as book keeping information for node. At any point the node data can be fetched and value can be extracted using the corresponding property name. Refer to
NXOpen.DataContainer
on how property name-value pair is added to the container or list.Signature
GetNodeData()
Returns: Node data which is list of property name - value pair. New property name - value pair can be added to it and existing value can be fetched using corresponding property name. Return type: NXOpen.DataContainer
New in version NX7.5.0.
License requirements: None.
GetState¶
-
Node.
GetState
¶ Gets the node state associated with node state icon.
Node state is an iconic representation, e.g., checked/unchecked icons for corresponding state. Node state value 1 and 2 represents the standard checked and unchecked state respectively.
Signature
GetState()
Returns: Node state Return type: int New in version NX7.5.0.
License requirements: None.
ScrollTo¶
-
Node.
ScrollTo
¶ Scrolls horizontally and vertically to make the specific column of node appear on the tree window.
Signature
ScrollTo(columnID, visibleOption)
Parameters: - columnID (int) – ColumnId of the column to which tree window scrolls horizontally.
- visibleOption (
NXOpen.BlockStyler.NodeScroll
) – Option to scroll the tree window vertically.
New in version NX7.5.0.
License requirements: None.
SetColumnDisplayText¶
-
Node.
SetColumnDisplayText
¶ Sets the text in the column which corresponds to given columnId.
The text is interpreted as icon if the column display type is
BlockStyler.TreeColumnDisplay.Icon
.Signature
SetColumnDisplayText(columnID, columnDisplayText)
Parameters: - columnID (int) – Unique coulmn id of the column.
- columnDisplayText (str) – Text associated with column
New in version NX7.5.0.
License requirements: None.
SetState¶
-
Node.
SetState
¶ Sets the node state which is associated with node state icon.
Node state is an iconic representation, e.g., checked/unchecked state. Setting node state to value other than 1 and 2 calls BlockStyler.Tree.StateIconName callback to fetch the icon name. Node state can be set only after the node has been added to TreeList.
Signature
SetState(state)
Parameters: state (int) – Node state New in version NX7.5.0.
License requirements: None.