NodeScroll Enumeration¶
NXOpen.BlockStyler.Node.Scroll is an alias for NXOpen.BlockStyler.NodeScroll
-
class
NXOpen.BlockStyler.
NodeScroll
¶ Bases:
object
Represents the scroll position to be applied on node.
Use one of these options to make the node appear in tree window.
Enum Members
Enum Member Enum Member Description Center Scrolls the tree to bring the node at the center of the tree window LeastScroll Scrolls the tree to minimal to make the node appear in tree window MostScroll Scrolls the tree to maximum to make the node appear in tree window -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-