NodeExpandOption Enumeration¶
NXOpen.BlockStyler.Node.ExpandOption is an alias for NXOpen.BlockStyler.NodeExpandOption
-
class
NXOpen.BlockStyler.
NodeExpandOption
¶ Bases:
object
Represents the Expand/Collapse option
Enum Members
Enum Member Enum Member Description Collapse Use this option to collapse the node. Expand Use this option to expand the node. The child node state is unaltered. Toggle Use this option to collapse the expanded node or expand the collapsed node. -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-