PmiLineWeldBuilder Class¶
-
class
NXOpen.Annotations.
PmiLineWeldBuilder
¶ Bases:
NXOpen.Annotations.LineWeldBuilder
Represents a
NXOpen.Annotations.PmiLineWeld
builderTo create a new instance of this class, use
NXOpen.Annotations.WeldCollection.CreatePmiLineWeldBuilder()
Default values.
Property Value FieldWeld Plain FlipDirection False FlipHorizontal False FlipVertical False IdLine Plain Scale 1 StaggeredWeld NoStaggeredSymbol Tail NoTail WeldAlongContour None New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
ArrowSideWeldData | Returns the NXOpen.Annotations.LineWeldDataBuilder for the arrow side of the weld symbol |
AssociatedObjects | Returns the NXOpen.Annotations.AssociatedObjectsBuilder for weld symbol |
FieldWeld | Returns or sets the field indicating the weld is done at the field site |
FlipDirection | Returns or sets the flip direction for top seam |
FlipHorizontal | Returns or sets the flip horizontal direction for side seam |
FlipVertical | Returns or sets the flip vertical direction for side seam |
ForeshorteningSymbol | Returns the foreshortening symbol builder |
IdLine | Returns or sets the identification or reference line |
Inherit | Returns the weld symbol from which the style properties are inherited |
Leader | Returns the NXOpen.Annotations.LeaderBuilder for weld symbol |
Origin | Returns the NXOpen.Annotations.OriginBuilder for the weld symbol |
OtherSideWeldData | Returns the NXOpen.Annotations.LineWeldDataBuilder for the other side of the weld symbol |
Scale | Returns or sets the scaling factor for the welding symbol |
SideSeamObjects | Returns the side seam object |
SpaceFactor | Returns or sets the space factor for the welding symbol |
StaggeredWeld | Returns or sets the staggered weld |
Style | Returns the NXOpen.Annotations.StyleBuilder for the weld symbol |
Tag | Returns the Tag for this object. |
Tail | Returns or sets the weld tail |
TopSeamObject | Returns the top seam object |
WeldAlongContour | Returns or sets the weld along contour option |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetReference | Returns the reference or specification text @return |
InheritProperties | This inherits the properties from the existing weld symbol |
InheritPropertiesFromWeldFeature | This inherits the properties from the existing weld feature |
SetReference | Sets the reference or specification text |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssociatedObjects¶
-
PmiLineWeldBuilder.
AssociatedObjects
¶ Returns the
NXOpen.Annotations.AssociatedObjectsBuilder
for weld symbol-------------------------------------
Getter Method
Signature
AssociatedObjects()
Returns: Return type: NXOpen.Annotations.AssociatedObjectsBuilder
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
PmiLineWeldBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.