AssociatedObjectsBuilder Class¶
-
class
NXOpen.Annotations.
AssociatedObjectsBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
The associated objects builder is used to store objects which annotations are associated to
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Nxobjects | Returns the associated NX objects |
Objects | Returns the associated objects |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Nxobjects¶
-
AssociatedObjectsBuilder.
Nxobjects
¶ Returns the associated NX objects
-------------------------------------
Getter Method
Signature
Nxobjects()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX9.0.0.
License requirements: None.
Objects¶
-
AssociatedObjectsBuilder.
Objects
¶ Returns the associated objects
-------------------------------------
Getter Method
Signature
Objects()
Returns: Return type: NXOpen.SelectDisplayableObjectList
New in version NX6.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Annotations.AssociatedObjectsBuilder.Nxobjects()
instead.License requirements: None.
Method Detail¶
Validate¶
-
AssociatedObjectsBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.