LineWeldDataBuilder Class¶
-
class
NXOpen.Annotations.
LineWeldDataBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.LineWeldDataBuilder
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
CompoundWeldSize | Returns or sets the compound weld size |
CompoundWeldSizeCode | Returns or sets the compound weld size letter code |
ContourSymbol | Returns or sets the supplementary contour weld symbols that identify the shape of the weld surface or execution of a weld for both top and bottom of the reference line |
FinishSymbol | Returns or sets the finishing method for the weld symbol |
GrooveCountersinkAngle | Returns or sets the groove or coutersink angle |
IsCompound | Returns or sets the compound weld |
LengthPitch | Returns or sets the length or pitch |
NumberRootDepth | Returns or sets the number of welds or root opening or depth of weld |
Tag | Returns the Tag for this object. |
WeldSize | Returns or sets the weld size |
WeldSizeCode | Returns or sets the weld size letter code |
WeldSymbol | Returns or sets the weld symbol |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
LineWeldDataBuilderContourSymbolType Enumeration | Represents the contour symbol type |
LineWeldDataBuilderFinishSymbolType Enumeration | Represents the finish symbol type. |
LineWeldDataBuilderWeldSizeCodeType Enumeration | Represents the weld size code type |
LineWeldDataBuilderWeldSymbolType Enumeration | Represents the weld symbol type |
Property Detail¶
CompoundWeldSize¶
-
LineWeldDataBuilder.
CompoundWeldSize
¶ Returns or sets the compound weld size
-------------------------------------
Getter Method
Signature
CompoundWeldSize()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CompoundWeldSize(compoundWeldSize)
Parameters: compoundWeldSize (str) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
CompoundWeldSizeCode¶
-
LineWeldDataBuilder.
CompoundWeldSizeCode
¶ Returns or sets the compound weld size letter code
-------------------------------------
Getter Method
Signature
CompoundWeldSizeCode()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilderWeldSizeCodeType
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CompoundWeldSizeCode(compoundWeldSizeCode)
Parameters: compoundWeldSizeCode ( NXOpen.Annotations.LineWeldDataBuilderWeldSizeCodeType
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
ContourSymbol¶
-
LineWeldDataBuilder.
ContourSymbol
¶ Returns or sets the supplementary contour weld symbols that identify the shape of the weld surface or execution of a weld for both top and bottom of the reference line
-------------------------------------
Getter Method
Signature
ContourSymbol()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilderContourSymbolType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ContourSymbol(contourSymbol)
Parameters: contourSymbol ( NXOpen.Annotations.LineWeldDataBuilderContourSymbolType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
FinishSymbol¶
-
LineWeldDataBuilder.
FinishSymbol
¶ Returns or sets the finishing method for the weld symbol
-------------------------------------
Getter Method
Signature
FinishSymbol()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilderFinishSymbolType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FinishSymbol(finishSymbol)
Parameters: finishSymbol ( NXOpen.Annotations.LineWeldDataBuilderFinishSymbolType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
GrooveCountersinkAngle¶
-
LineWeldDataBuilder.
GrooveCountersinkAngle
¶ Returns or sets the groove or coutersink angle
-------------------------------------
Getter Method
Signature
GrooveCountersinkAngle()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GrooveCountersinkAngle(grooveCountersinkAngle)
Parameters: grooveCountersinkAngle (str) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
IsCompound¶
-
LineWeldDataBuilder.
IsCompound
¶ Returns or sets the compound weld
-------------------------------------
Getter Method
Signature
IsCompound()
Returns: Return type: bool New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsCompound(isCompound)
Parameters: isCompound (bool) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
LengthPitch¶
-
LineWeldDataBuilder.
LengthPitch
¶ Returns or sets the length or pitch
-------------------------------------
Getter Method
Signature
LengthPitch()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LengthPitch(lengthPitch)
Parameters: lengthPitch (str) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
NumberRootDepth¶
-
LineWeldDataBuilder.
NumberRootDepth
¶ Returns or sets the number of welds or root opening or depth of weld
-------------------------------------
Getter Method
Signature
NumberRootDepth()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NumberRootDepth(numberRootDepth)
Parameters: numberRootDepth (str) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
WeldSize¶
-
LineWeldDataBuilder.
WeldSize
¶ Returns or sets the weld size
-------------------------------------
Getter Method
Signature
WeldSize()
Returns: Return type: str New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WeldSize(weldSize)
Parameters: weldSize (str) – New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
WeldSizeCode¶
-
LineWeldDataBuilder.
WeldSizeCode
¶ Returns or sets the weld size letter code
-------------------------------------
Getter Method
Signature
WeldSizeCode()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilderWeldSizeCodeType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WeldSizeCode(weldSizeCode)
Parameters: weldSizeCode ( NXOpen.Annotations.LineWeldDataBuilderWeldSizeCodeType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
WeldSymbol¶
-
LineWeldDataBuilder.
WeldSymbol
¶ Returns or sets the weld symbol
-------------------------------------
Getter Method
Signature
WeldSymbol()
Returns: Return type: NXOpen.Annotations.LineWeldDataBuilderWeldSymbolType
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
WeldSymbol(weldSymbol)
Parameters: weldSymbol ( NXOpen.Annotations.LineWeldDataBuilderWeldSymbolType
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Method Detail¶
Validate¶
-
LineWeldDataBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.