LineWeldDataBuilderFinishSymbolType Enumeration

NXOpen.Annotations.LineWeldDataBuilder.FinishSymbolType is an alias for NXOpen.Annotations.LineWeldDataBuilderFinishSymbolType

class NXOpen.Annotations.LineWeldDataBuilderFinishSymbolType

Bases: object

Represents the finish symbol type.

Enum Members

Enum Member Enum Member Description
NotSet
Chipping  
Grinding  
Hammering  
Machining  
Rolling  
Peening  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.