LineWeldDataBuilderWeldSizeCodeType Enumeration

NXOpen.Annotations.LineWeldDataBuilder.WeldSizeCodeType is an alias for NXOpen.Annotations.LineWeldDataBuilderWeldSizeCodeType

class NXOpen.Annotations.LineWeldDataBuilderWeldSizeCodeType

Bases: object

Represents the weld size code type

Enum Members

Enum Member Enum Member Description
NotSet  
A  
C  
D  
S  
Z  
P  
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.