PmiCenterMarkBuilder Class¶
-
class
NXOpen.Annotations.
PmiCenterMarkBuilder
¶ Bases:
NXOpen.Annotations.BaseCenterMarkBuilder
Builder for creating PMI Center Mark.
It creates or edits PMI Center Marks To create a new instance of this class, use
NXOpen.Annotations.CenterlineCollection.CreatePmiCenterMarkBuilder()
Default values.
Property Value MultipleCenterMarks false New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AssociatedObjects | Returns the associated objects for the center mark |
Locations | Returns the location object |
MultipleCenterMarks | Returns or sets the multiple center marks option, applicable only for creation |
Plane | Returns the plane for the creation of center mark |
Settings | Returns the center mark settings builder |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddEndExtensions | Adds extensions only at ends |
AddExtension | Adds extension based on select object index |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllExtensions | Returns all extensions. |
GetAllIndividualExtensions | Returns individual extensions. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetEndExtensions | Returns end extensions only. |
GetObject | Returns the object currently being edited by this builder. |
RemoveEndExtensions | Removes extensions only at ends |
RemoveExtension | Removes extension based on select object index |
RemoveLocation | Removes location object for a given index from the Select Object List. |
ResetAllExtensions | Reset all extensions by the supplied defaultValue |
SetAllIndividualExtensions | Sets all individual extensions |
SetEndExtensions | Modifies end extensions only |
SetIndividualExtensions | Modifies extensions based on select object index |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
AssociatedObjects¶
-
PmiCenterMarkBuilder.
AssociatedObjects
¶ Returns the associated objects for the center mark
-------------------------------------
Getter Method
Signature
AssociatedObjects()
Returns: Return type: NXOpen.Annotations.AssociatedObjectsBuilder
New in version NX7.5.0.
License requirements: None.
Plane¶
-
PmiCenterMarkBuilder.
Plane
¶ Returns the plane for the creation of center mark
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.Annotations.PlaneBuilder
New in version NX7.5.0.
License requirements: None.
Method Detail¶
Validate¶
-
PmiCenterMarkBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.