BaseCenterMarkBuilder Class

class NXOpen.Annotations.BaseCenterMarkBuilder

Bases: NXOpen.Annotations.CenterlineBuilder

Represents a Base CenterMark Builder for Pmi and Drafting centermark

This is an abstract class, and cannot be instantiated.

Default values.

Property Value
Settings.Angle 0
Settings.Extension 6.35 (millimeters part), 0.25 (inches part)
Settings.Gap 1.5875 (millimeters part), 0.0625 (inches part)
Settings.IndividualDistance 0
Settings.InheritAngle 0
Settings.ShowCenterPoint 0
Settings.Size 3.175 (millimeters part), 0.125 (inches part)
Settings.Width Thin

New in version NX7.5.0.

Properties

Property Description
Locations Returns the location object
MultipleCenterMarks Returns or sets the multiple center marks option, applicable only for creation
Settings Returns the center mark settings builder
Tag Returns the Tag for this object.

Methods

Method Description
AddEndExtensions Adds extensions only at ends
AddExtension Adds extension based on select object index
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetAllExtensions Returns all extensions.
GetAllIndividualExtensions Returns individual extensions.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetEndExtensions Returns end extensions only.
GetObject Returns the object currently being edited by this builder.
RemoveEndExtensions Removes extensions only at ends
RemoveExtension Removes extension based on select object index
RemoveLocation Removes location object for a given index from the Select Object List.
ResetAllExtensions Reset all extensions by the supplied defaultValue
SetAllIndividualExtensions Sets all individual extensions
SetEndExtensions Modifies end extensions only
SetIndividualExtensions Modifies extensions based on select object index
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

Locations

BaseCenterMarkBuilder.Locations

Returns the location object

-------------------------------------

Getter Method

Signature Locations()

Returns:
Return type:NXOpen.SelectNXObjectList

New in version NX6.0.0.

License requirements: None.

MultipleCenterMarks

BaseCenterMarkBuilder.MultipleCenterMarks

Returns or sets the multiple center marks option, applicable only for creation

-------------------------------------

Getter Method

Signature MultipleCenterMarks()

Returns:
Return type:bool

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature MultipleCenterMarks(multipleCenterlines)

Parameters:multipleCenterlines (bool) –

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)

Settings

BaseCenterMarkBuilder.Settings

Returns the center mark settings builder

-------------------------------------

Getter Method

Signature Settings()

Returns:
Return type:NXOpen.Annotations.CenterMarkSettingsBuilder

New in version NX6.0.0.

License requirements: None.

Method Detail

RemoveLocation

BaseCenterMarkBuilder.RemoveLocation

Removes location object for a given index from the Select Object List.

This method is required for the retained centermark case, however the method can be used for removing any object from select object list for the CenterMark

Signature RemoveLocation(index)

Parameters:index (int) – Index of the object in the select object list

New in version NX6.0.0.

License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)

Validate

BaseCenterMarkBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.