OrdinateDimensionBuilder Class¶
-
class
NXOpen.Annotations.
OrdinateDimensionBuilder
¶ Bases:
NXOpen.Annotations.BaseOrdinateDimensionBuilder
Represents a
NXOpen.Annotations.OrdinateDimension
builderTo create a new instance of this class, use
NXOpen.Annotations.DimensionCollection.CreateOrdinateDimensionBuilder()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ActiveHorizontalMargin | Returns or sets the active horizontal margin(defined or inferred) where horizontal dimension will be automatically placed. |
ActiveVerticalMargin | Returns or sets the active vertical margin(defined or inferred) where horizontal dimension will be automatically placed. |
AllowDuplicates | Returns or sets the allow duplicates |
AppendedText | Returns the appended text |
AutoAssociativities | Returns the auto ordinate associativities |
Baseline | Returns the baseline |
Driving | Returns the driving |
ForeshorteningSymbol | Returns the foreshortening symbol builder |
HorizontalInferredMarginLocation | Returns or sets the horizontal inferred margin location |
Inherit | Returns the inherit |
OrdinateOrigin | Returns the ordinate origin |
Origin | Returns the origin |
RespositionExisting | Returns or sets the resposition existing |
SecondAssociativities | Returns the second associativities |
Style | Returns the style |
Tag | Returns the Tag for this object. |
Type | Returns or sets the type |
VerticalInferredMarginLocation | Returns or sets the vertical inferred margin location |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Driving¶
-
OrdinateDimensionBuilder.
Driving
¶ Returns the driving
-------------------------------------
Getter Method
Signature
Driving()
Returns: Return type: NXOpen.Annotations.DrivingValueBuilder
New in version NX9.0.0.
License requirements: None.
ForeshorteningSymbol¶
-
OrdinateDimensionBuilder.
ForeshorteningSymbol
¶ Returns the foreshortening symbol builder
-------------------------------------
Getter Method
Signature
ForeshorteningSymbol()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
OrdinateDimensionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.