ForeshorteningSymbolBuilder Class¶
-
class
NXOpen.Annotations.
ForeshorteningSymbolBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a
NXOpen.Annotations.ForeshorteningSymbolBuilder
builderThere is no KF creator for this class.
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
AddSymbol | Add the foreshortening symbol |
DeleteSymbol | Delete the foreshortening symbol |
GetSymbols | Get the foreshortening symbol @return |
ModifySymbol | Modify the foreshortening symbol |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AddSymbol¶
-
ForeshorteningSymbolBuilder.
AddSymbol
¶ Add the foreshortening symbol
Signature
AddSymbol(locations)
Parameters: locations ( NXOpen.Point3d
) –New in version NX10.0.0.
License requirements: None.
DeleteSymbol¶
-
ForeshorteningSymbolBuilder.
DeleteSymbol
¶ Delete the foreshortening symbol
Signature
DeleteSymbol(symbolIndex)
Parameters: symbolIndex (int) – New in version NX10.0.0.
License requirements: None.
GetSymbols¶
-
ForeshorteningSymbolBuilder.
GetSymbols
¶ Get the foreshortening symbol
Signature
GetSymbols()
Returns: a tuple Return type: A tuple consisting of (locations, indices). locations is a list of NXOpen.Point3d
. indices is a list of int.New in version NX10.0.0.
License requirements: None.
ModifySymbol¶
-
ForeshorteningSymbolBuilder.
ModifySymbol
¶ Modify the foreshortening symbol
Signature
ModifySymbol(symbolIndex, locations)
Parameters: - symbolIndex (int) –
- locations (
NXOpen.Point3d
) –
New in version NX10.0.0.
License requirements: None.
Validate¶
-
ForeshorteningSymbolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.