BaseOrdinateDimensionBuilder Class

class NXOpen.Annotations.BaseOrdinateDimensionBuilder

Bases: NXOpen.Builder

Represents a NXOpen.Annotations.OrdinateDimension builder

This is an abstract class and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
ActiveHorizontalMargin Returns or sets the active horizontal margin(defined or inferred) where horizontal dimension will be automatically placed.
ActiveVerticalMargin Returns or sets the active vertical margin(defined or inferred) where horizontal dimension will be automatically placed.
AllowDuplicates Returns or sets the allow duplicates
AppendedText Returns the appended text
AutoAssociativities Returns the auto ordinate associativities
Baseline Returns the baseline
HorizontalInferredMarginLocation Returns or sets the horizontal inferred margin location
Inherit Returns the inherit
OrdinateOrigin Returns the ordinate origin
Origin Returns the origin
RespositionExisting Returns or sets the resposition existing
SecondAssociativities Returns the second associativities
Style Returns the style
Tag Returns the Tag for this object.
Type Returns or sets the type
VerticalInferredMarginLocation Returns or sets the vertical inferred margin location

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

BaseOrdinateDimensionBuilderTypes Enumeration the type of dimension being created

Property Detail

ActiveHorizontalMargin

BaseOrdinateDimensionBuilder.ActiveHorizontalMargin

Returns or sets the active horizontal margin(defined or inferred) where horizontal dimension will be automatically placed.

A margin can be created using NXOpen.Annotations.OrdinateMarginCollection. If None, must set a HorizontalInferredMarginLocation which will be used to place dimension

-------------------------------------

Getter Method

Signature ActiveHorizontalMargin()

Returns:
Return type:NXOpen.Annotations.OrdinateMargin

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ActiveHorizontalMargin(margin)

Parameters:margin (NXOpen.Annotations.OrdinateMargin) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

ActiveVerticalMargin

BaseOrdinateDimensionBuilder.ActiveVerticalMargin

Returns or sets the active vertical margin(defined or inferred) where horizontal dimension will be automatically placed.

A margin can be created using NXOpen.Annotations.OrdinateMarginCollection. If None, must set a VerticalInferredMarginLocation which will be used to place dimension

-------------------------------------

Getter Method

Signature ActiveVerticalMargin()

Returns:
Return type:NXOpen.Annotations.OrdinateMargin

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ActiveVerticalMargin(margin)

Parameters:margin (NXOpen.Annotations.OrdinateMargin) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

AllowDuplicates

BaseOrdinateDimensionBuilder.AllowDuplicates

Returns or sets the allow duplicates

-------------------------------------

Getter Method

Signature AllowDuplicates()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AllowDuplicates(allowDuplicates)

Parameters:allowDuplicates (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

AppendedText

BaseOrdinateDimensionBuilder.AppendedText

Returns the appended text

-------------------------------------

Getter Method

Signature AppendedText()

Returns:
Return type:NXOpen.Annotations.AppendedTextBuilder

New in version NX9.0.0.

License requirements: None.

AutoAssociativities

BaseOrdinateDimensionBuilder.AutoAssociativities

Returns the auto ordinate associativities

-------------------------------------

Getter Method

Signature AutoAssociativities()

Returns:
Return type:NXOpen.SelectDisplayableObjectList

New in version NX9.0.0.

License requirements: None.

Baseline

BaseOrdinateDimensionBuilder.Baseline

Returns the baseline

-------------------------------------

Getter Method

Signature Baseline()

Returns:
Return type:NXOpen.Annotations.OrdinateBaselineBuilder

New in version NX9.0.0.

License requirements: None.

HorizontalInferredMarginLocation

BaseOrdinateDimensionBuilder.HorizontalInferredMarginLocation

Returns or sets the horizontal inferred margin location

-------------------------------------

Getter Method

Signature HorizontalInferredMarginLocation()

Returns:
Return type:NXOpen.Point3d

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature HorizontalInferredMarginLocation(location)

Parameters:location (NXOpen.Point3d) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Inherit

BaseOrdinateDimensionBuilder.Inherit

Returns the inherit

-------------------------------------

Getter Method

Signature Inherit()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

OrdinateOrigin

BaseOrdinateDimensionBuilder.OrdinateOrigin

Returns the ordinate origin

-------------------------------------

Getter Method

Signature OrdinateOrigin()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Origin

BaseOrdinateDimensionBuilder.Origin

Returns the origin

-------------------------------------

Getter Method

Signature Origin()

Returns:
Return type:NXOpen.Annotations.OriginBuilder

New in version NX9.0.0.

License requirements: None.

RespositionExisting

BaseOrdinateDimensionBuilder.RespositionExisting

Returns or sets the resposition existing

-------------------------------------

Getter Method

Signature RespositionExisting()

Returns:
Return type:bool

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature RespositionExisting(respositionExisting)

Parameters:respositionExisting (bool) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

SecondAssociativities

BaseOrdinateDimensionBuilder.SecondAssociativities

Returns the second associativities

-------------------------------------

Getter Method

Signature SecondAssociativities()

Returns:
Return type:NXOpen.SelectDisplayableObject

New in version NX9.0.0.

License requirements: None.

Style

BaseOrdinateDimensionBuilder.Style

Returns the style

-------------------------------------

Getter Method

Signature Style()

Returns:
Return type:NXOpen.Annotations.StyleBuilder

New in version NX9.0.0.

License requirements: None.

Type

BaseOrdinateDimensionBuilder.Type

Returns or sets the type

-------------------------------------

Getter Method

Signature Type()

Returns:
Return type:NXOpen.Annotations.BaseOrdinateDimensionBuilderTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(type)

Parameters:type (NXOpen.Annotations.BaseOrdinateDimensionBuilderTypes) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

VerticalInferredMarginLocation

BaseOrdinateDimensionBuilder.VerticalInferredMarginLocation

Returns or sets the vertical inferred margin location

-------------------------------------

Getter Method

Signature VerticalInferredMarginLocation()

Returns:
Return type:NXOpen.Point3d

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature VerticalInferredMarginLocation(location)

Parameters:location (NXOpen.Point3d) –

New in version NX9.0.0.

License requirements: drafting (“DRAFTING”)

Method Detail

Validate

BaseOrdinateDimensionBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.