BaseOrdinateDimensionBuilderTypes Enumeration

NXOpen.Annotations.BaseOrdinateDimensionBuilder.Types is an alias for NXOpen.Annotations.BaseOrdinateDimensionBuilderTypes

class NXOpen.Annotations.BaseOrdinateDimensionBuilderTypes

Bases: object

the type of dimension being created

Enum Members

Enum Member Enum Member Description
SingleDimension
singular dimension
MultipleDimension
group or set of dimensions
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.