MasterSymbolBuilder Class¶
-
class
NXOpen.Annotations.
MasterSymbolBuilder
¶ Bases:
NXOpen.Builder
Represents a Builder for MasterSymbol functionality
To create a new instance of this class, use
NXOpen.Annotations.CustomSymbolCollection.CreateMasterSymbolBuilder()
Default values.
Property Value ImageCapture.CaptureMethod GraphicsArea ImageCapture.Format Bmp ImageCapture.Size Pixels64 New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
AnchorPoint | Returns or sets the anchor point |
Contents | Returns the select object |
ImageCapture | Returns the image capture builder |
ImageName | Returns or sets the symbol image name |
ItemName | Returns or sets the Item Name, valid in team center |
ItemNumber | Returns or sets the item number, valid in team center |
NoteList | Returns the note list |
PartFileName | Returns or sets the part file name |
Revision | Returns or sets the revision, valid in team center |
SymbolName | Returns or sets the JA method support for accessing and setting Symbol Name value |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateNewListItem | Create Master Symbol list item builder @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
EditImage | Changes symbol image |
GenerateItemNumber | Item number assign button. |
GenerateRevision | Revision assign button, This will generate the revision number, valid in team center |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetLeaderAttachmentPoint | Getting Leader attachment point from builder side @return |
GetMultilineString | Returns the multiple notes for a given Text Type. |
GetObject | Returns the object currently being edited by this builder. |
GetPartOperationCreateBuilder | Gets NXOpen.PDM.PartOperationBuilder @return |
Rename | Renames symbol |
SetIsPartSymbol | Sets if it is part symbol |
SetLeaderAttachmentPoint | Setting Leader attachment point on builder side |
SetPartOperationCreateBuilder | Sets NXOpen.PDM.PartOperationBuilder |
SetPath | Setting Path retrieved from Global method at builder side |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
MasterSymbolBuilderLeaderAttachmentType Enumeration | The Enum for Attachment options |
Property Detail¶
AnchorPoint¶
-
MasterSymbolBuilder.
AnchorPoint
¶ Returns or sets the anchor point
-------------------------------------
Getter Method
Signature
AnchorPoint()
Returns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AnchorPoint(anchorPoint)
Parameters: anchorPoint ( NXOpen.Point
) –New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Contents¶
-
MasterSymbolBuilder.
Contents
¶ Returns the select object
-------------------------------------
Getter Method
Signature
Contents()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.5.0.
License requirements: None.
ImageCapture¶
-
MasterSymbolBuilder.
ImageCapture
¶ Returns the image capture builder
-------------------------------------
Getter Method
Signature
ImageCapture()
Returns: Return type: NXOpen.Gateway.ImageCaptureBuilder
New in version NX7.5.0.
License requirements: None.
ImageName¶
-
MasterSymbolBuilder.
ImageName
¶ Returns or sets the symbol image name
-------------------------------------
Getter Method
Signature
ImageName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ImageName(imageName)
Parameters: imageName (str) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
ItemName¶
-
MasterSymbolBuilder.
ItemName
¶ Returns or sets the Item Name, valid in team center
-------------------------------------
Getter Method
Signature
ItemName()
Returns: Return type: str New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ItemName(itemName)
Parameters: itemName (str) – New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder
instead.License requirements: drafting (“DRAFTING”)
ItemNumber¶
-
MasterSymbolBuilder.
ItemNumber
¶ Returns or sets the item number, valid in team center
-------------------------------------
Getter Method
Signature
ItemNumber()
Returns: Return type: str New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
ItemNumber(itemNumber)
Parameters: itemNumber (str) – New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder
instead.License requirements: drafting (“DRAFTING”)
NoteList¶
-
MasterSymbolBuilder.
NoteList
¶ Returns the note list
-------------------------------------
Getter Method
Signature
NoteList()
Returns: Return type: NXOpen.NXObjectList
New in version NX7.5.0.
License requirements: None.
PartFileName¶
-
MasterSymbolBuilder.
PartFileName
¶ Returns or sets the part file name
-------------------------------------
Getter Method
Signature
PartFileName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PartFileName(partFileName)
Parameters: partFileName (str) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Revision¶
-
MasterSymbolBuilder.
Revision
¶ Returns or sets the revision, valid in team center
-------------------------------------
Getter Method
Signature
Revision()
Returns: Return type: str New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
Revision(revision)
Parameters: revision (str) – New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.PDM.PartOperationCreateBuilder
instead.License requirements: drafting (“DRAFTING”)
SymbolName¶
-
MasterSymbolBuilder.
SymbolName
¶ Returns or sets the JA method support for accessing and setting Symbol Name value
-------------------------------------
Getter Method
Signature
SymbolName()
Returns: Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolName(symbolName)
Parameters: symbolName (str) – New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Method Detail¶
CreateNewListItem¶
-
MasterSymbolBuilder.
CreateNewListItem
¶ Create Master Symbol list item builder
Signature
CreateNewListItem(noteTag, notes)
Parameters: - noteTag (
NXOpen.Annotations.Annotation
) – - notes (list of str) – name of the solution
Returns: Return type: New in version NX7.5.0.
License requirements: None.
- noteTag (
EditImage¶
-
MasterSymbolBuilder.
EditImage
¶ Changes symbol image
Signature
EditImage(currentSymbolTag, newImageName)
Parameters: - currentSymbolTag (
NXOpen.Annotations.MasterSymbol
) – symbol Tag - newImageName (str) – New image name
New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
- currentSymbolTag (
GenerateItemNumber¶
-
MasterSymbolBuilder.
GenerateItemNumber
¶ Item number assign button.
This will generate the item number, valid in team center
Signature
GenerateItemNumber()
New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Annotations.MasterSymbolBuilder.ItemNumber()
instead.License requirements: drafting (“DRAFTING”)
GenerateRevision¶
-
MasterSymbolBuilder.
GenerateRevision
¶ Revision assign button, This will generate the revision number, valid in team center
Signature
GenerateRevision()
New in version NX7.5.0.
Deprecated since version NX10.0.0: Use
NXOpen.Annotations.MasterSymbolBuilder.Revision()
instead.License requirements: drafting (“DRAFTING”)
GetLeaderAttachmentPoint¶
-
MasterSymbolBuilder.
GetLeaderAttachmentPoint
¶ Getting Leader attachment point from builder side
Signature
GetLeaderAttachmentPoint(attachmentType)
Parameters: attachmentType ( NXOpen.Annotations.MasterSymbolBuilderLeaderAttachmentType
) – Attachment type either of left or rightReturns: Return type: NXOpen.Point
New in version NX7.5.0.
License requirements: None.
GetMultilineString¶
-
MasterSymbolBuilder.
GetMultilineString
¶ Returns the multiple notes for a given Text Type.
This property is valid if
NXOpen.Annotations.MasterSymbolListItemBuilder.TextType()
is either of controlled, partially controlled or arbitorySignature
GetMultilineString()
Returns: Multiple notes as Output Return type: list of str New in version NX7.5.0.
License requirements: None.
GetPartOperationCreateBuilder¶
-
MasterSymbolBuilder.
GetPartOperationCreateBuilder
¶ Gets
NXOpen.PDM.PartOperationBuilder
Signature
GetPartOperationCreateBuilder()
Returns: Return type: NXOpen.PDM.PartOperationCreateBuilder
New in version NX10.0.0.
License requirements: None.
Rename¶
-
MasterSymbolBuilder.
Rename
¶ Renames symbol
Signature
Rename(currentSymbolTag, newSymbolName)
Parameters: - currentSymbolTag (
NXOpen.Annotations.MasterSymbol
) – symbol Tag - newSymbolName (str) – New symbol name
New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
- currentSymbolTag (
SetIsPartSymbol¶
-
MasterSymbolBuilder.
SetIsPartSymbol
¶ Sets if it is part symbol
Signature
SetIsPartSymbol(isPartSymbol)
Parameters: isPartSymbol (bool) – True If it is part symbol New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
SetLeaderAttachmentPoint¶
-
MasterSymbolBuilder.
SetLeaderAttachmentPoint
¶ Setting Leader attachment point on builder side
Signature
SetLeaderAttachmentPoint(attachmentType, leaderAttachmentPoint)
Parameters: - attachmentType (
NXOpen.Annotations.MasterSymbolBuilderLeaderAttachmentType
) – Attachment type either of left or right - leaderAttachmentPoint (
NXOpen.Point
) – Attachment point
New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
- attachmentType (
SetPartOperationCreateBuilder¶
-
MasterSymbolBuilder.
SetPartOperationCreateBuilder
¶ Sets
NXOpen.PDM.PartOperationBuilder
Signature
SetPartOperationCreateBuilder(partOperationBuilder)
Parameters: partOperationBuilder ( NXOpen.PDM.PartOperationCreateBuilder
) –New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
SetPath¶
-
MasterSymbolBuilder.
SetPath
¶ Setting Path retrieved from Global method at builder side
Signature
SetPath(path)
Parameters: path (str) – location of symbol New in version NX7.5.0.
License requirements: drafting (“DRAFTING”)
Validate¶
-
MasterSymbolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.