MasterSymbolBuilderLeaderAttachmentType Enumeration

NXOpen.Annotations.MasterSymbolBuilder.LeaderAttachmentType is an alias for NXOpen.Annotations.MasterSymbolBuilderLeaderAttachmentType

class NXOpen.Annotations.MasterSymbolBuilderLeaderAttachmentType

Bases: object

The Enum for Attachment options

Enum Members

Enum Member Enum Member Description
Left
Left Attachment
Right
Right Attachment
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.