IdSymbolBuilder Class¶
-
class
NXOpen.Annotations.
IdSymbolBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.Annotations.IdSymbol
builderTo create a new instance of this class, use
NXOpen.Annotations.IdSymbolCollection.CreateIdSymbolBuilder()
Default values.
Property Value Size 0 New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ForeshorteningSymbol | Returns the foreshortening symbol builder |
Inherit | Returns the inherit The id symbol from which the style properties are inherited |
Leader | Returns the NXOpen.Annotations.LeaderBuilder for the annotation |
LowerText | Returns or sets the lower text The text displayed in the lower portion of the divided symbol In case Quadrant Circle symbol, the lower text is placed in the lower right quadrant just above the horizontal dividing line. |
Origin | Returns the origin, where the symbol is going to be displayed |
Placement | Returns an annotation placement object |
Size | Returns or sets the size The circle symbols are measured by diameter, the rounded box is measured by length, and all other symbols are measured by a circumscribed circle |
Style | Returns the style |
SymbolType | Returns or sets the symbol type |
Tag | Returns the Tag for this object. |
Type | Returns or sets the symbol type |
UpperText | Returns or sets the upper text The text displayed in the upper portion of the divided symbol In case Quadrant Circle symbol, the upper text is placed in the upper left quadrant just above the horizontal dividing line. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetPreviewObject | Sets the preview object for dialog creation of id symbols |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
IdSymbolBuilderSymbolTypes Enumeration | the valid types for an id symbol |
Property Detail¶
ForeshorteningSymbol¶
-
IdSymbolBuilder.
ForeshorteningSymbol
¶ Returns the foreshortening symbol builder
-------------------------------------
Getter Method
Signature
ForeshorteningSymbol()
Returns: Return type: NXOpen.Annotations.ForeshorteningSymbolBuilder
New in version NX10.0.0.
License requirements: None.
Inherit¶
-
IdSymbolBuilder.
Inherit
¶ Returns the inherit The id symbol from which the style properties are inherited
-------------------------------------
Getter Method
Signature
Inherit()
Returns: Return type: NXOpen.SelectObject
New in version NX5.0.0.
License requirements: None.
Leader¶
-
IdSymbolBuilder.
Leader
¶ Returns the
NXOpen.Annotations.LeaderBuilder
for the annotation-------------------------------------
Getter Method
Signature
Leader()
Returns: Return type: NXOpen.Annotations.LeaderBuilder
New in version NX6.0.0.
License requirements: None.
LowerText¶
-
IdSymbolBuilder.
LowerText
¶ Returns or sets the lower text The text displayed in the lower portion of the divided symbol In case Quadrant Circle symbol, the lower text is placed in the lower right quadrant just above the horizontal dividing line.
-------------------------------------
Getter Method
Signature
LowerText()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerText(lowerText)
Parameters: lowerText (str) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Origin¶
-
IdSymbolBuilder.
Origin
¶ Returns the origin, where the symbol is going to be displayed
-------------------------------------
Getter Method
Signature
Origin()
Returns: Return type: NXOpen.Annotations.OriginBuilder
New in version NX6.0.0.
License requirements: None.
Placement¶
-
IdSymbolBuilder.
Placement
¶ Returns an annotation placement object
-------------------------------------
Getter Method
Signature
Placement()
Returns: Return type: NXOpen.Annotations.AnnotationPlacement
New in version NX5.0.0.
Deprecated since version NX6.0.0: This functionality is no longer supported.
License requirements: None.
Size¶
-
IdSymbolBuilder.
Size
¶ Returns or sets the size The circle symbols are measured by diameter, the rounded box is measured by length, and all other symbols are measured by a circumscribed circle
-------------------------------------
Getter Method
Signature
Size()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Size(size)
Parameters: size (float) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Style¶
-
IdSymbolBuilder.
Style
¶ Returns the style
-------------------------------------
Getter Method
Signature
Style()
Returns: Return type: NXOpen.Annotations.StyleBuilder
New in version NX6.0.0.
License requirements: None.
SymbolType¶
-
IdSymbolBuilder.
SymbolType
¶ Returns or sets the symbol type
-------------------------------------
Getter Method
Signature
SymbolType()
Returns: Return type: NXOpen.Annotations.IdSymbolBuilderSymbolTypes
New in version NX5.0.0.
Deprecated since version NX6.0.0: Use
NXOpen.Annotations.IdSymbolBuilder.Type()
instead.License requirements: None.
-------------------------------------
Setter Method
Signature
SymbolType(symbolType)
Parameters: symbolType ( NXOpen.Annotations.IdSymbolBuilderSymbolTypes
) –New in version NX5.0.0.
Deprecated since version NX6.0.0: Use
NXOpen.Annotations.IdSymbolBuilder.Type()
instead.License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Type¶
-
IdSymbolBuilder.
Type
¶ Returns or sets the symbol type
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.Annotations.IdSymbolBuilderSymbolTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(type)
Parameters: type ( NXOpen.Annotations.IdSymbolBuilderSymbolTypes
) –New in version NX6.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
UpperText¶
-
IdSymbolBuilder.
UpperText
¶ Returns or sets the upper text The text displayed in the upper portion of the divided symbol In case Quadrant Circle symbol, the upper text is placed in the upper left quadrant just above the horizontal dividing line.
-------------------------------------
Getter Method
Signature
UpperText()
Returns: Return type: str New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperText(upperText)
Parameters: upperText (str) – New in version NX5.0.0.
License requirements: drafting (“DRAFTING”) OR geometric_tol (“GDT”)
Method Detail¶
SetPreviewObject¶
-
IdSymbolBuilder.
SetPreviewObject
¶ Sets the preview object for dialog creation of id symbols
Signature
SetPreviewObject(symbol)
Parameters: symbol ( NXOpen.Annotations.IdSymbol
) – rubberbanding symbolNew in version NX5.0.0.
Deprecated since version NX6.0.0: This functionality is no longer supported.
License requirements: None.
Validate¶
-
IdSymbolBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.