IdSymbolBuilderSymbolTypes Enumeration¶
NXOpen.Annotations.IdSymbolBuilder.SymbolTypes is an alias for NXOpen.Annotations.IdSymbolBuilderSymbolTypes
-
class
NXOpen.Annotations.
IdSymbolBuilderSymbolTypes
¶ Bases:
object
the valid types for an id symbol
Enum Members
Enum Member Enum Member Description Circle CircleDividedCircle Divided circleTriangle Triangle with point downTriangleUp Triangle with point upSquare SquareDividedSquare Divided squareHexagon HexagonDividedHexagon Divided hexagonQuadrantCircle Quadrant circleRoundedBox Rounded boxUnderline Underline-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-