/*
uf_draw_types.h
File description:
Contains Open C API s and macros that are specific to the DRAW module.
*****************************************************************************/
#ifndef UF_DRAW_TYPES_INCLUDED
#define UF_DRAW_TYPES_INCLUDED
/***************************************************************************
***************************************************************************/
#include <uf_drf_types.h>
#include <uf_object_types.h>
#define UF_DRAW_NUM_VIEW_PARMS 9
#define UF_DRAW_MAX_NUM_SXSEGS 99
#define UF_DRAW_MAX_NUM_STEP_SXSEGS 49
#define UF_DRAW_MAX_LABEL_LEN (132)
/*************************************************************************
Section through components attribute name:
This is the user-defined string attribute title.
A string value of yes is the default. Components are sectioned.
A string value of no indicates that the component is not sectioned.
For more information, reference the Drafting User's Manual.
**************************************************************************/
#define UF_DRAW_SECTION_ATTR "section-component"
/*************************************************************************
Curve for Hidden Line Removal attribute name:
This is the user-defined string attribute title.
A string value of yes is to allow the curve to join the process of
Hidden Line Removal.
A string value of no indicates that the curve is not to join the process
of Hidden Line Removal.
For more information, reference the Drafting User's Manual.
**************************************************************************/
#define UF_DRAW_CURVE_HLR_ATTR "DMV_HLR"
/*******************************************************************************
Attribute name for the curve for Hidden Line Processing:
This is the user-defined attribute of Null type.
If this attribute is assigned to a curve, The curve will be ignored during
Hidden Line Processing.
The curves without this attribute will participate during Hidden Line Processing.
********************************************************************************/
#define UF_DRAW_CURVE_HLP_ATTR "DMV_HLP_IGNORE"
/*************************************************************************
Arrow head types
*************************************************************************/
enum UF_DRAW_arw_head_type_e
{
UF_DRAW_ansi_arrow = 1,
UF_DRAW_iso_arrow,
UF_DRAW_iso128,
UF_DRAW_jis,
UF_DRAW_gb
};
typedef enum UF_DRAW_arw_head_type_e UF_DRAW_arw_head_type_t;
/*************************************************************************
Arrow head control (style)
Figure. Arrowhead Style, Open, Closed and Filled
*************************************************************************/
enum UF_DRAW_arw_head_cntl_e
{
UF_DRAW_closed_arrowhead = 1,
UF_DRAW_open_arrowhead,
UF_DRAW_filled_arrowhead
};
typedef enum UF_DRAW_arw_head_cntl_e UF_DRAW_arw_head_cntl_t;
/*************************************************************************
Section line segment type
*************************************************************************/
enum UF_DRAW_sxseg_type_e
{
UF_DRAW_sxseg_arrow = UF_arrow_segment_subtype,
UF_DRAW_sxseg_cut = UF_cut_segment_subtype,
UF_DRAW_sxseg_bend = UF_bend_segment_subtype
};
typedef enum UF_DRAW_sxseg_type_e UF_DRAW_sxseg_type_t;
/*************************************************************************
Revolved section line leg
*************************************************************************/
enum UF_DRAW_sxline_leg_e
{
UF_DRAW_sxline_leg1 = 1,
UF_DRAW_sxline_leg2
};
typedef enum UF_DRAW_sxline_leg_e UF_DRAW_sxline_leg_t;
/*************************************************************************
Section line status
**************************************************************************/
enum UF_DRAW_sxline_status_e
{
UF_DRAW_invalid_sxline = 0, /*
status may require that a segment be
added with UF_DRAW_add_sxline_sxseg
*/
UF_DRAW_valid_sxline, /* section line is valid */
UF_DRAW_sxline_sxseg_lost_assoc, /* warning, at least one segment
of section line lost associativity
*/
UF_DRAW_sxline_rotpt_lost_assoc, /* warning, section line rotation
point lost associativity
*/
UF_DRAW_sxline_rotpt_or_sxseg_lost_assoc /*
warning, section line rotation
point lost associativity and at
least one segment of section
line lost associativity
*/
};
typedef enum UF_DRAW_sxline_status_e UF_DRAW_sxline_status_t;
/************************************************************************
Section line display
*************************************************************************/
enum UF_DRAW_sxline_display_e
{
UF_DRAW_no_display_sxline = 1,
UF_DRAW_display_sxline
};
typedef enum UF_DRAW_sxline_display_e UF_DRAW_sxline_display_t;
/**************************************************************************
Section line segment mode
**************************************************************************/
enum UF_DRAW_sxseg_mode_e
{
UF_DRAW_user_defined_sxseg = 1,
UF_DRAW_system_defined_sxseg
};
typedef enum UF_DRAW_sxseg_mode_e UF_DRAW_sxseg_mode_t;
/*************************************************************************
Section line type
*************************************************************************/
enum UF_DRAW_sxline_type_e
{
UF_DRAW_simple_sxline = 1,
UF_DRAW_stepped_sxline,
UF_DRAW_revolved_sxline,
UF_DRAW_half_sxline,
UF_DRAW_unfolded_sxline,
UF_DRAW_breakline,
UF_DRAW_folded_sxline
};
typedef enum UF_DRAW_sxline_type_e UF_DRAW_sxline_type_t;
/*************************************************************************
Section segment highlight status
**************************************************************************/
enum UF_DRAW_sxseg_highlight_e
{
UF_DRAW_unhighlighted = 0,
UF_DRAW_highlighted
};
typedef enum UF_DRAW_sxseg_highlight_e UF_DRAW_sxseg_highlight_t;
/************************************************************************
Arrow parameters structure for section line display
*************************************************************************/
typedef struct UF_DRAW_arrow_parms_s *UF_DRAW_arrow_parms_p_t;
struct UF_DRAW_arrow_parms_s {
double size; /* Arrow size must be greater than 0.
Figure Arrow Display Sizes (A in the figure)
*/
double total_length; /* Arrow total length (must be
greater than 0)
*/
double incl_angle; /* Arrow included angle
(must be greater than 0)
*/
double past_part_dist; /* Arrow past part
(must be greater than 0)
Figure Arrow Past Part Distance
*/
double stub_len; /* Arrow stub length
(must be greater than 0)
Figure Stub Length
*/
UF_DRAW_arw_head_type_t head_type; /* Arrow head type
UF_DRAW_ansi_arrow = ansi arrow
UF_DRAW_iso_arrow = iso arrow
Figure Ansi vs. ISO arrow head types
*/
UF_DRAW_arw_head_cntl_t head_control; /* Arrow head control (style)
(must be greater than 0)
UF_DRAW_open_arrowhead
UF_DRAW_closed_arrowhead
UF_DRAW_filled_arrowhead
Figure Arrowhead Style
*/
} ;
typedef struct UF_DRAW_arrow_parms_s UF_DRAW_arrow_parms_t;
/**************************************************************************
Half section line segment object structure
**************************************************************************/
typedef struct UF_DRAW_half_sxsegs_s *UF_DRAW_half_sxsegs_p_t;
struct UF_DRAW_half_sxsegs_s {
UF_DRF_object_p_t bend_object; /* Object associated to bend segment*/
UF_DRF_object_p_t cut_object; /* Object associated to cut segment */
UF_DRF_object_p_t arrow_object; /* Object associated to arrow
segment */
} ;
typedef struct UF_DRAW_half_sxsegs_s UF_DRAW_half_sxsegs_t;
/*************************************************************************
Section line segment object structure used for revolved, stepped
and unfolded section line types.
*************************************************************************/
typedef struct UF_DRAW_sxline_sxsegs_s *UF_DRAW_sxline_sxsegs_p_t;
struct UF_DRAW_sxline_sxsegs_s {
UF_DRAW_sxseg_type_t sxseg_type; /* UF_DRAW_sxseg_arrow = arrow segment
UF_DRAW_sxseg_cut = cut segment
UF_DRAW_sxseg_bend = bend segment
*/
UF_DRF_object_p_t sxseg_object; /* Object associated to section line segment */
double sxseg_angle; /* Angle of section segment in degrees from
-180 to 180 (for unfolded section line
segments only)
*/
} ;
typedef struct UF_DRAW_sxline_sxsegs_s UF_DRAW_sxline_sxsegs_t;
/*************************************************************************
Section line segment structure
**************************************************************************/
struct UF_DRAW_sxseg_info_s
{
UF_DRAW_sxseg_type_t sxseg_type; /* Segment type:
UF_DRAW_sxseg_arrow = arrow segment
UF_DRAW_sxseg_cut = cut segment
UF_DRAW_sxseg_bend = bend segment
*/
UF_DRAW_sxline_leg_t leg_num; /* Segment leg number:
If REVOLVED Section Line, then leg_num
can be UF_DRAW_sxline_leg1 or
UF_DRAW_sxline_leg2. In all other cases
it will be UF_DRAW_sxline_leg1.
*/
UF_DRAW_sxseg_mode_t sxseg_mode; /* Creation mode of segment:
UF_DRAW_system_defined_sxseg
UF_DRAW_user_defined_sxseg
*/
UF_DRAW_sxseg_highlight_t highlight_status; /* Segment highlight state
(due to lost associativity)
UF_DRAW_unhighlighted
UF_DRAW_highlighted
*/
double sxseg_angle; /* Angle of segment (for unfolded section
line segments only). In degrees from
-180 to 180.
*/
} ;
typedef struct UF_DRAW_sxseg_info_s UF_DRAW_sxseg_info_t;
typedef struct UF_DRAW_sxseg_info_s *UF_DRAW_sxseg_info_p_t;
/*************************************************************************
Section view Section Sheet Bodies status
**************************************************************************/
enum UF_DRAW_sx_section_sheet_body_e
{
UF_DRAW_sx_section_sheet_body_off = 0,
UF_DRAW_sx_section_sheet_body_on
} ;
typedef enum UF_DRAW_sx_section_sheet_body_e UF_DRAW_sx_section_sheet_body_t;
/*************************************************************************
Section view background status
**************************************************************************/
enum UF_DRAW_sx_background_e
{
UF_DRAW_sx_background_off = 0,
UF_DRAW_sx_background_on
} ;
typedef enum UF_DRAW_sx_background_e UF_DRAW_sx_background_t;
/**************************************************************************
Section view crosshatch status
**************************************************************************/
enum UF_DRAW_sx_crosshatch_e
{
UF_DRAW_sx_crosshatch_off = 0,
UF_DRAW_sx_crosshatch_on
} ;
typedef enum UF_DRAW_sx_crosshatch_e UF_DRAW_sx_crosshatch_t;
/*************************************************************************
Section view assembly crosshatching status
**************************************************************************/
enum UF_DRAW_sx_assy_xhatch_e
{
UF_DRAW_sx_assy_xhatch_off = 0,
UF_DRAW_sx_assy_xhatch_on
} ;
typedef enum UF_DRAW_sx_assy_xhatch_e UF_DRAW_sx_assy_xhatch_t;
/**************************************************************************
Hidden line removal status
**************************************************************************/
enum UF_DRAW_hidden_line_e
{
UF_DRAW_hidden_line_removal_off = 0,
UF_DRAW_hidden_line_removal_on
} ;
typedef enum UF_DRAW_hidden_line_e UF_DRAW_hidden_line_t;
/*************************************************************************
Hidden edge status
**************************************************************************/
enum UF_DRAW_edge_hiding_edge_e
{
UF_DRAW_edge_hiding_edge_off = 0,
UF_DRAW_edge_hiding_edge_on
} ;
typedef enum UF_DRAW_edge_hiding_edge_e UF_DRAW_edge_hiding_edge_t;
/**************************************************************************
Edge smooth status
**************************************************************************/
enum UF_DRAW_smooth_e
{
UF_DRAW_smooth_off = 0,
UF_DRAW_smooth_on
} ;
typedef enum UF_DRAW_smooth_e UF_DRAW_smooth_t;
/*************************************************************************
Silhouette status
**************************************************************************/
enum UF_DRAW_silhouette_e
{
UF_DRAW_silhouettes_off = 0,
UF_DRAW_silhouettes_on
} ;
typedef enum UF_DRAW_silhouette_e UF_DRAW_silhouette_t;
/*************************************************************************
UV Hatch status
**************************************************************************/
enum UF_DRAW_uvhatch_e
{
UF_DRAW_uvhatch_off = 0,
UF_DRAW_uvhatch_on
} ;
typedef enum UF_DRAW_uvhatch_e UF_DRAW_uvhatch_t;
/*************************************************************************
Smooth Edge Gap status
**************************************************************************/
enum UF_DRAW_gap_e
{
UF_DRAW_gap_off = 0,
UF_DRAW_gap_on
} ;
typedef enum UF_DRAW_gap_e UF_DRAW_gap_t;
/**************************************************************************
Virtual Intersection Curve status
**************************************************************************/
enum UF_DRAW_virtual_intersect_e
{
UF_DRAW_virtual_intersect_off = 0,
UF_DRAW_virtual_intersect_on
} ;
typedef enum UF_DRAW_virtual_intersect_e UF_DRAW_virtual_intersect_t;
/**************************************************************************
Extracted edge status - should edges be extracted for the view?
**************************************************************************/
enum UF_DRAW_extracted_edges_e
{
UF_DRAW_extracted_edges_off = 0,
UF_DRAW_extracted_edges_on
} ;
typedef enum UF_DRAW_extracted_edges_e UF_DRAW_extracted_edges_t;
/**************************************************************************
drafting curve type
**************************************************************************/
enum UF_DRAW_drafting_curve_type_e
{
UF_DRAW_unknown_type = -1,
UF_DRAW_extracted_edge_type = 1,
UF_DRAW_silhouette_curve_type,
UF_DRAW_thread_silhouette_curve_type,
UF_DRAW_section_edge_type,
UF_DRAW_thread_section_edge_type,
UF_DRAW_vi_curve_type,
UF_DRAW_uvhatch_curve_type,
UF_DRAW_trace_line_type,
UF_DRAW_simplified_curve_type,
UF_DRAW_interference_curve_type,
UF_DRAW_extracted_model_curve_type
};
typedef enum UF_DRAW_drafting_curve_type_e UF_DRAW_drafting_curve_type_t;
/**************************************************************************
Section view structure
**************************************************************************/
typedef struct UF_DRAW_sxview_prfs_s *UF_DRAW_sxview_prfs_p_t;
struct UF_DRAW_sxview_prfs_s
{
UF_DRAW_sx_section_sheet_body_t sx_section_sheet_body;
/* Section view
Section Sheet Body
UF_DRAW_sx_section_sheet_body_off
UF_DRAW_sx_section_sheet_body_on
*/
UF_DRAW_sx_background_t sx_background; /* Section view background
UF_DRAW_sx_background_on
UF_DRAW_sx_background_off
*/
UF_DRAW_sx_crosshatch_t sx_crosshatch; /* Section view crosshatch
UF_DRAW_sx_crosshatch_off
UF_DRAW_sx_crosshatch_on
*/
UF_DRAW_sx_assy_xhatch_t sx_assy_xhatch;
double xhatch_adj_toler;
};
typedef struct UF_DRAW_sxview_prfs_s UF_DRAW_sxview_prfs_t;
/*****************************************************************************
View display preferences structure
******************************************************************************/
typedef struct UF_DRAW_view_prfs_s *UF_DRAW_view_prfs_p_t;
struct UF_DRAW_view_prfs_s
{
UF_DRAW_hidden_line_t hidden_line; /* Hidden line removal, use
UF_DRAW_hidden_line_removal_off or
UF_DRAW_hidden_line_removal_on
*/
int hidden_line_color; /* Hidden line color
*/
int hidden_line_font; /* Hidden line font
*/
int hidden_line_width; /* Hidden line width,
please use
UF_OBJ_WIDTH_NORMAL,
UF_OBJ_WIDTH_THIN,
UF_OBJ_WIDTH_THICK, or
UF_OBJ_WIDTH_ORIGINAL
*/
UF_DRAW_edge_hiding_edge_t edge_hiding_edge; /*
UF_DRAW_edge_hiding_edge_off or
UF_DRAW_edge_hiding_edge_on
*/
UF_DRAW_smooth_t smooth; /* Smooth Edges UF_DRAW_smooth_off or
UF_DRAW_smooth_on
*/
double tolerance; /* Chord height tolerance for
silhouettes and hidden line
display; must be >= 0.0
*/
UF_DRAW_silhouette_t silhouettes; /* UF_DRAW_silhouettes_off or
UF_DRAW_silhouettes_on
*/
UF_DRAW_uvhatch_t uvhatch; /* UF_DRAW_uvhatch_off or
UF_DRAW_uvhatch_on
*/
int smooth_edge_color; /* Smooth edge color
(0=original)
*/
int smooth_edge_font; /* Smooth edge font
(0=original)
*/
int smooth_edge_width; /* Smooth edge width
(see hidden_line_width)
*/
UF_DRAW_gap_t smooth_edge_gap; /* Smooth edge gap
(0=off, 1 = on)
*/
double smooth_edge_gap_size; /* Smooth edge gap
size (in part units)
*/
UF_DRAW_virtual_intersect_t virtual_intersect; /* Virtual intersection
curves (0=off, 1 = on)
*/
int virtual_intersect_color;/* Virtual
intersection color
(0=original)
*/
int virtual_intersect_font; /* Virtual
intersection font
(0=original)
*/
int virtual_intersect_width;/* Virtual
intersection width
(0=original)
*/
UF_DRAW_gap_t virtual_intersect_gap;
double virtual_intersect_gap_size;
UF_DRAW_extracted_edges_t extracted_edges; /* Associative Extracted
Edge use (0=off, 1=on)
*/
int visible_line_color; /* (0 = original) */
int visible_line_font; /* (0=original) */
int visible_line_width; /* Please use either
UF_OBJ_WIDTH_NORMAL,
UF_OBJ_WIDTH_THIN,
UF_OBJ_WIDTH_THICK, or
UF_OBJ_WIDTH_ORIGINAL
*/
int interfering_solids; /* 0 = no interfering solids
1 = yes without Interference Curves
2 = yes and render InterferenceCurves
*/
logical referenced_edges_only; /* When TRUE, renders only hidden lines
referencing annotation with hidden line
settings above. When FALSE, all hidden
lines are rendered with hidden line
settings above.
*/
logical edges_hidden_by_own_solid; /* When TRUE, renders self-hidden
edges according to hidden line
settings above. When FALSE, only
edges hidden by other solids are
rendered according to hidden line
settings above.
*/
int simplify_small_features; /* 0 = don't simplify
1 = simplify features
smaller than small_feature_tolerance
when rendering hidden lines.
2 = hide features small than the
small_feature_tolerance when
rendering hidden lines.
*/
double small_feature_tolerance; /* Small feature tolerance percentage
(from 0.0 to 5.00). Features
smaller than this percentage of the
model will be simplified when
simplify_small_features is true.
*/
int traceline_visible_color; /* Traceline visible color
(0=original)
*/
int traceline_visible_font; /* Traceline visible font
(0=original)
*/
int traceline_visible_width; /* Traceline visible width
(see hidden_line_width)
*/
int traceline_hidden_color; /* Traceline hidden color
(0=original)
*/
int traceline_hidden_font; /* Traceline hidden font
(0=invisible)
*/
int traceline_hidden_width; /* Traceline hidden width
(see hidden_line_width)
*/
UF_DRAW_gap_t traceline_gap; /* Traceline gap
(0=off, 1 = on)
*/
double traceline_gap_size; /* Traceline gap
size (in part units)
*/
} ;
typedef struct UF_DRAW_view_prfs_s UF_DRAW_view_prfs_t;
/****************************************************************************
* The following enum defines the rendering methods for all of the threads
* in a given view.
*****************************************************************************/
enum UF_DRAW_thd_meth_e
{
UF_DRAW_THD_METH_NONE=0, /* No method specified (default for pre-v12 parts)
*/
UF_DRAW_THD_METH_ANSI_SIMPLIFIED, /* Render threads using the ANSI
* standard simplified method
*/
UF_DRAW_THD_METH_ANSI_SCHEMATIC, /* Render threads using the ANSI
* standard schematic method
*/
UF_DRAW_THD_METH_ANSI_DETAILED, /* Render threads using the ANSI
* standard detailed method
*/
UF_DRAW_THD_METH_ISO_SIMPLIFIED, /* Render threads using the ISO
*standard simplified method
*/
UF_DRAW_THD_METH_ISO_DETAILED, /* Render thread using the ISO
* standard detailed method
*/
UF_DRAW_THD_METH_ESKD_SIMPLIFIED /* Render thread using the
* ESKD standard.
*/
};
typedef enum UF_DRAW_thd_meth_e UF_DRAW_thd_meth_t;
/*************************************************************************
View Boundary structure - used for asking boundary curves and
making a view boundary associative to the model.
**************************************************************************/
struct UF_DRAW_view_boundary_s {
tag_t curve_tag; /* Tag of boundary curve. */
logical const_status; /* Construction status of a curve.
FALSE = not a construction line
TRUE = curve is a construction line
This parameter is unused when defining a
view boundary (you cannot define a view
boundary with a construction curve with
NX Open API).
*/
int point_count; /* Number of defining points for the curve.*/
tag_p_t defining_points; /* Array of defining points for the curve */
tag_t hatch_tag; /* Tag of hatch object */
};
typedef struct UF_DRAW_view_boundary_s UF_DRAW_view_boundary_t,
*UF_DRAW_view_boundary_p_t;
/**************************************************************************
Define View Boundary structure - setting a break line detail type
view boundary.
*************************************************************************/
struct UF_DRAW_define_boundary_s {
tag_t curve_tag; /* Tag of curve defining the
view boundary. */
};
typedef struct UF_DRAW_define_boundary_s UF_DRAW_define_boundary_t,
*UF_DRAW_define_boundary_p_t;
/**************************************************************************
Drawing Sizes
**************************************************************************/
enum UF_DRAW_metric_size_e
{
UF_DRAW_A0 = 1, /* 841 x 1189 */
UF_DRAW_A1, /* 594 X 841 */
UF_DRAW_A2, /* 420 X 594 */
UF_DRAW_A3, /* 297 X 420 */
UF_DRAW_A4 /* 210 X 297 */
};
typedef enum UF_DRAW_metric_size_e UF_DRAW_metric_size_t;
enum UF_DRAW_english_size_e
{
UF_DRAW_A = 1, /* 8.5 x 11 */
UF_DRAW_B, /* 11 X 17 */
UF_DRAW_C, /* 17 X 22 */
UF_DRAW_D, /* 22 X 34 */
UF_DRAW_E, /* 34 X 44 */
UF_DRAW_F, /* 28 X 40 */
UF_DRAW_H, /* 28 X 44 */
UF_DRAW_J /* 34 X 55 */
};
typedef enum UF_DRAW_english_size_e UF_DRAW_english_size_t;
union UF_DRAW_size_union_u
{
UF_DRAW_metric_size_t metric_size_code;
UF_DRAW_english_size_t english_size_code;
double custom_size[2];
};
typedef union UF_DRAW_size_union_u UF_DRAW_size_union_t;
enum UF_DRAW_size_state_e
{
UF_DRAW_METRIC_SIZE = 0,
UF_DRAW_ENGLISH_SIZE,
UF_DRAW_CUSTOM_SIZE
};
typedef enum UF_DRAW_size_state_e UF_DRAW_size_state_t;
/*************************************************************************
Projection Angles
**************************************************************************/
enum UF_DRAW_projection_angle_e
{
UF_DRAW_NO_ANGLE_DATA = 0,
UF_DRAW_THIRD_ANGLE_PROJECTION,
UF_DRAW_FIRST_ANGLE_PROJECTION
};
typedef enum UF_DRAW_projection_angle_e UF_DRAW_projection_angle_t;
/**************************************************************************
View Status for Adding Views
**************************************************************************/
enum UF_DRAW_view_status_e
{
UF_DRAW_ACTIVE_VIEW = 1,
UF_DRAW_REFERENCE_VIEW
};
typedef enum UF_DRAW_view_status_e UF_DRAW_view_status_t;
/*************************************************************************
Boundary types
**************************************************************************/
enum UF_DRAW_boundary_type_e
{
UF_DRAW_BREAK_DETAIL_TYPE = 1,
UF_DRAW_MANUAL_RECTANGLE_TYPE,
UF_DRAW_AUTOMATIC_RECTANGLE_TYPE,
UF_DRAW_BOUND_BY_OBJECTS_TYPE
};
typedef enum UF_DRAW_boundary_type_e UF_DRAW_boundary_type_t;
/**************************************************************************
Orthographic Projection Direction
**************************************************************************/
enum UF_DRAW_proj_dir_e
{
UF_DRAW_project_infer = 0,
UF_DRAW_project_above,
UF_DRAW_project_right,
UF_DRAW_project_below,
UF_DRAW_project_left
};
typedef enum UF_DRAW_proj_dir_e UF_DRAW_proj_dir_t;
/**************************************************************************
Drawing Info Structure
**************************************************************************/
typedef struct UF_DRAW_info_s *UF_DRAW_info_p_t;
struct UF_DRAW_info_s{
UF_DRAW_size_state_t size_state; /* Flag specifying the type used in
size, UF_DRAW_METRIC_SIZE,
UF_DRAW_ENGLISH_SIZE or
UF_DRAW_CUSTOM_SIZE. */
UF_DRAW_size_union_t size; /* The drawing size, as specified in
size_state. If using metric,
then use a UF_DRAW_metric_size_t
variable. If using english, use
a UF_DRAW_english_size_t
variable. If using a custom size,
specify the size in a double array
where size[0] is the height and
size[1] is the length.
*/
double drawing_scale; /* The drawing scale. */
int units; /* The drawing units, either
UF_PART_METRIC or UF_PART_ENGLISH. */
UF_DRAW_projection_angle_t projection_angle; /* The projection angle, either
UF_DRAW_THIRD_ANGLE_PROJECTION or
UF_DRAW_FIRST_ANGLE_PROJECTION.
*/
};
typedef struct UF_DRAW_info_s UF_DRAW_info_t;
/**************************************************************************
Drawing Member View Structure
**************************************************************************/
typedef struct UF_DRAW_view_info_s *UF_DRAW_view_info_p_t;
struct UF_DRAW_view_info_s{
UF_DRAW_view_status_t view_status; /* Active = UF_DRAW_ACTIVE_VIEW,
reference = UF_DRAW_REFERENCE_VIEW.
*/
tag_t anchor_point; /* The anchor point of the view. Must
be a smart point (see uf_so.h).
When adding a view, if no anchor
point is desired, use NULL_TAG. If
you wish to set the view reference
point with a "dumb" point, use
uc6484.
*/
double view_scale; /* The view scale. */
logical use_ref_pt; /* If true, then used the saved
reference point. */
logical clean_model_view; /* v15.0 No longer used, model
views can no longer be cleaned
when imported onto a drawing */
logical inherit_boundary; /* If TRUE, then the drawing view
will inherit the model view's
boundary. */
logical transfer_annotation; /* If TRUE, annotations are
moved from model view to
imported drawing view */
logical inherit_pmi; /* If TRUE, then PMI are copied
from the model view to the
imported drawing view */
char model_name[UF_DRAW_MAX_LABEL_LEN]; /* Part name for the view, filespec with path, may be '\0'.
Used only when importing views
or asking the settings of a view */
char arrangement_name[UF_DRAW_MAX_LABEL_LEN]; /* Name of arrangement, may be '\0'.
Used only when importing views, or
asking the settings of a view. */
};
typedef struct UF_DRAW_view_info_s UF_DRAW_view_info_t;
/******************************************************************************
* Render Set display preferences structure
*
******************************************************************************/
typedef struct UF_DRAW_render_prefs_s *UF_DRAW_render_prefs_p_t;
struct UF_DRAW_render_prefs_s
{
UF_DRAW_hidden_line_t hidden_line; /* Hidden line rendering */
int hidden_line_color; /* Hidden line color
(0=original) */
int hidden_line_font; /* Hidden line font
(0=original) */
int hidden_line_width; /* Hidden line width, use
UF_OBJ_WIDTH_NORMAL
UF_OBJ_WIDTH_THIN
UF_OBJ_WIDTH_THICK
UF_OBJ_WIDTH_ORIGINAL */
UF_DRAW_edge_hiding_edge_t edge_hiding_edge; /* UF_DRAW_edge_hiding_edge_off
UF_DRAW_edge_hiding_edge_on
*/
int visible_line_color; /* Visible line color
(0=original) */
int visible_line_font; /* Visible line font
(0=original) */
int visible_line_width; /* Visible line width, use
UF_OBJ_WIDTH_NORMAL
UF_OBJ_WIDTH_THIN
UF_OBJ_WIDTH_THICK
UF_OBJ_WIDTH_ORIGINAL */
logical referenced_edges_only; /* When TRUE, renders only hidden lines
referencing annotation with hidden
line settings above. When FALSE, all
hidden lines are rendered with
hidden line settings above.
*/
logical edges_hidden_by_own_solid; /* When TRUE, renders self-hidden
edges according to hidden line
settings above. When FALSE, only
edges hidden by other solids
are rendered according to hidden
line settings above.
*/
};
typedef struct UF_DRAW_render_prefs_s UF_DRAW_render_prefs_t;
/* Pen assignment for plot data. */
enum UF_DRAW_pen_assignment_e
{
UF_DRAW_USE_CURRENT_VALUE = 0,
UF_DRAW_DENSITY,
UF_DRAW_COLOR
};
typedef enum UF_DRAW_pen_assignment_e UF_DRAW_pen_assignment_t;
/* Data source for plot data. */
enum UF_DRAW_data_source_e
{
UF_DRAW_DRAWING_DATA = 0,
UF_DRAW_DEFAULT_DATA
};
typedef enum UF_DRAW_data_source_e UF_DRAW_data_source_t;
/**************************************************************************
* Drawing Plotter Data Structure
**************************************************************************/
typedef struct UF_DRAW_plotter_data_s *UF_DRAW_plotter_data_p_t;
struct UF_DRAW_plotter_data_s
{
char plotter_name[17]; /* Plotter name (16 characters max). */
double plot_scale; /* Plot scale. */
double rotation; /* Rotation angle (in degrees).*/
int media_ref_num; /* Media reference number. */
int copies; /* Number of copies. */
double plot_origin[2]; /* Plot origin (XY coordinates).
[0] - X coordinate
[1] - Y coordinate */
double plot_offset[2]; /* Plot offset (XY coordinates).
[0] - X offset
[1] - Y offset */
UF_DRAW_pen_assignment_t pen_assignment; /* Pen assignment.
UF_DRAW_DENSITY
UF_DRAW_COLOR */
int pen_list[16]; /* Pen list. */
UF_DRAW_data_source_t data_source; /* Data source.
UF_DRAW_DRAWING_DATA
UF_DRAW_DEFAULT_DATA */
} ;
typedef struct UF_DRAW_plotter_data_s UF_DRAW_plotter_data_t;
/* Sectioning component in view settings. */
enum UF_DRAW_comp_section_in_view_e
{
UF_DRAW_NON_SECTIONED = 0,
UF_DRAW_SECTIONED,
UF_DRAW_NOT_VIEW_SPECIFIED
};
typedef enum UF_DRAW_comp_section_in_view_e UF_DRAW_comp_section_in_view_t;
/* Breakout section data structure. */
struct UF_DRAW_breakout_data_s
{
tag_t base_point; /* Base point on the floor of breakout */
tag_t extrusion_vector; /* If NULL_TAG, the extrusion vector is
perpendicular to the xy plane of the
view and points toward the viewer.
Otherwise, the vector is perpendicular
to the floor of the breakout section
and points toward the side of the floor
on which the material of the part is
removed. */
int num_curves; /* Number of breakout curves */
tag_p_t curves; /* Breakout curves */
logical *const_status; /* Construction status of each
breakout curve */
logical cut_thru_model; /* Cut through the model */
logical hidden_line_hatching; /* Hidden line hatching */
};
typedef struct UF_DRAW_breakout_data_s
UF_DRAW_breakout_data_t, *UF_DRAW_breakout_data_p_t;
/* break region positioning mehods */
enum UF_DRAW_break_position_type_e
{
UF_DRAW_BREAK_POSITION_INFERRED = 0,
UF_DRAW_BREAK_POSITION_DISTANCE,
UF_DRAW_BREAK_POSITION_TWO_REGIONS,
UF_DRAW_BREAK_POSITION_DEFAULT
};
typedef enum UF_DRAW_break_position_type_e UF_DRAW_break_position_type_t;
/* Breakout section data structure. */
struct UF_DRAW_break_region_data_s
{
tag_t view_tag; /* Tag of broken view */
UF_DRAW_break_position_type_t position_type;
/* Positioning method */
double distance; /* Distance (gap) between aligned XY boxes
of break region and reference region in
drawing units; for inferred and
distance position types only */
tag_t reference_regions[2]; /* Break region(s) to be used as reference
for alignment */
tag_t alignment_vectors[2]; /* Direction(s) of alignment in drawing
coordinates */
};
typedef struct UF_DRAW_break_region_data_s
UF_DRAW_break_region_data_t, *UF_DRAW_break_region_data_p_t;
/* Break Region boundary structure */
struct UF_DRAW_break_region_boundary_s {
tag_t curve_tag; /* Tag of curve defining the break region
boundary */
logical construction_curve; /* TRUE if hidden; FALSE if visible */
logical hatch_curve; /* TRUE if curve is to be hatched; FALSE
if not */
};
typedef struct UF_DRAW_break_region_boundary_s
UF_DRAW_break_region_boundary_t, *UF_DRAW_break_region_boundary_p_t;
/* view label parameter type */
enum UF_DRAW_view_label_parm_type_t
{
UF_DRAW_view_label_other_view = 1,
UF_DRAW_view_label_detail_view ,
UF_DRAW_view_label_section_view,
UF_DRAW_view_label_projected_view
};
/* view label view label type - use view name or prefix and letter */
enum UF_DRAW_view_label_view_text_type_t
{
UF_DRAW_view_label_view_name = 1,
UF_DRAW_view_label_prefix_and_letter
};
/* view label letter format */
enum UF_DRAW_view_label_letter_format_t
{
UF_DRAW_view_label_single_letter = 1,
UF_DRAW_view_label_dashed_letter
};
/* view label scale position relative to view label */
enum UF_DRAW_view_label_scale_position_t
{
UF_DRAW_view_label_below = 1, /* scale label is below view label */
UF_DRAW_view_label_above, /* scale label is above view label */
UF_DRAW_view_label_before, /* scale label is before view label */
UF_DRAW_view_label_after /* scale label is after view label */
};
/* view label position relative to view boundary */
enum UF_DRAW_view_label_position_t
{
UF_DRAW_view_label_below_boundary = 1,
UF_DRAW_view_label_above_boundary
};
/* view label scale format */
enum UF_DRAW_view_label_scale_format_t
{
UF_DRAW_view_label_ratio = 1,
UF_DRAW_view_label_vertical_fraction,
UF_DRAW_view_label_horizontal_fraction,
UF_DRAW_view_label_Nx
};
/* view label on parent type - used for detail views */
enum UF_DRAW_label_on_parent_type_t
{
UF_DRAW_parent_view_label_no_display = 0, /* no circle */
UF_DRAW_parent_view_label_boundary, /* circle */
UF_DRAW_parent_view_label_circle = UF_DRAW_parent_view_label_boundary, /* alternate name for circle */
UF_DRAW_parent_view_label_note, /* circle with note */
UF_DRAW_parent_view_label_label, /* circle with label */
UF_DRAW_parent_view_label_embedded, /* embedded note in circle */
UF_DRAW_parent_view_label_true_boundary /* true boundary */
};
/* view label text to stub format option - used for detail views */
enum UF_DRF_view_label_text_to_stub_format_t
{
UF_DRAW_parent_view_label_text_before_stub = 0,
UF_DRAW_parent_view_label_text_above_stub
};
/* Secondary indexing alignment */
enum UF_DRAW_secondary_indexing_align_t
{
UF_DRAW_secondary_indexing_inline = 0,
UF_DRAW_secondary_indexing_subscript
};
#define UF_DRAW_MAX_LETTER_NCHARS 30
#define UF_DRAW_MAX_LETTER_BUFSIZE NX_BUFSIZE(UF_DRAW_MAX_LETTER_NCHARS)
/* */
#define UF_DRAW_MAX_LETTER_LEN (UF_DRAW_MAX_LETTER_BUFSIZE-1)
/* */
/* view label preferences */
struct UF_DRAW_view_label_parms_s {
UF_DRAW_view_label_parm_type_t view_label_parm_type;
/* Parameter type - Detail view,
Section View, or other. */
UF_DRAW_view_label_view_text_type_t view_label_type;
/* View label type - view name or
view letter */
UF_DRAW_view_label_letter_format_t letter_format;
/* Letter format - single letter or
letter separated by dash */
UF_DRAW_view_label_position_t view_label_position;
/* View Label position relative to
view boundary */
UF_DRAW_view_label_scale_position_t view_scale_position;
/* View Scale position relative to
view label */
UF_DRAW_view_label_scale_format_t view_scale_value_format;
/* View Scale value format - ratio,
vertical fraction, horizontal
fraction, or Nx */
UF_DRF_view_label_text_to_stub_format_t view_label_text_to_stub_format;
/* View lable text to stub format -
controls the location of the text
on the parent view label relative
to the stub. */
double letter_size_factor; /* Character size of letter relative
to the current font */
double view_scale_prefix_factor; /* Character size of scale label
relative to the current font */
double view_scale_text_factor; /* Character size of scale value
relative to the current font */
logical view_label; /* TRUE - include view label;
FALSE - do not include view label
*/
logical scale_label; /* TRUE - include scale label;
FALSE - do not include scale label
*/
logical view_label_customize; /* TRUE - turn on customized toggle
FALSE - turn off customized toggle
*/
logical scale_parentheses; /* TRUE - include parentheses around scale;
FALSE - do not include parentheses around scale;
*/
char view_label_prefix[UF_DRAW_MAX_LABEL_LEN];
/* View label prefix string */
char scale_label_prefix[UF_DRAW_MAX_LABEL_LEN];
/* Scale label prefix string */
char view_letter[UF_DRAW_MAX_LETTER_BUFSIZE];
/* View letter string */
UF_DRAW_label_on_parent_type_t parent_label_type;
/* label on parent of detail view type */
double text_to_gap_factor; /* Defines how big the gap will be for embedded
label on parent types */
char parent_vw_lbl_prefix[UF_DRAW_MAX_LABEL_LEN];
/* Parent view label prefix string */
logical show_rotation_symbol; /* Show rotation symbol */
logical show_rotation_angle; /* Show rotation angle */
UF_DRAW_secondary_indexing_align_t secondary_indexing_align; /* Secondary indexing alignment */
double subscript_size_factor; /* Subscript size factor */
};
typedef struct UF_DRAW_view_label_parms_s
UF_DRAW_view_label_parms_t, *UF_DRAW_view_label_parms_p_t;
#endif /* UF_DRAW_TYPES_INCLUDED */