UF_DRAW_view_boundary_s (view source)
 
Defined in: uf_draw_types.h
 
Also known as:
 
Overview
View Boundary structure - used for asking boundary curves and
making a view boundary associative to the model.


Data Members

curve_tag
tag_t
Tag of boundary curve.

const_status
logical
Construction status of a curve.
FALSE = not a construction line
TRUE = curve is a construction line
This parameter is unused when defining a
view boundary (you cannot define a view
boundary with a construction curve with
NX Open API).

point_count
int
Number of defining points for the curve.

defining_points
tag_p_t
Array of defining points for the curve

hatch_tag
tag_t
Tag of hatch object