UF_DRAW_breakout_data_s (view source)
 
Defined in: uf_draw_types.h
 
Also known as:
 
Overview
Breakout section data structure.


Data Members

base_point
tag_t
Base point on the floor of breakout

extrusion_vector
tag_t
If NULL_TAG, the extrusion vector is
perpendicular to the xy plane of the
view and points toward the viewer.
Otherwise, the vector is perpendicular
to the floor of the breakout section
and points toward the side of the floor
on which the material of the part is
removed.

num_curves
int
Number of breakout curves

curves
tag_p_t
Breakout curves

const_status
logical *
Construction status of each
breakout curve

cut_thru_model
logical
Cut through the model

hidden_line_hatching
logical
Hidden line hatching