Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Field and Description |
---|---|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.BEAD
Bead command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.COMPOUND
Compound Weld command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.DATUM_LOCATOR
Datum Locator command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.DATUM_PIN
Datum Pin command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.DATUM_SURFACE
Datum Surface command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.EASY_MEASUREMENT_PATTERN
Easy Measurement Pattern command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.EASY_SPOT
Easy Spot command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.FILL
Fill command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.FILLET
Fillet Weld command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.GROOVE
Groove Weld command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.IMPORT_CSV
Import CSV command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.JOINT
Welding Joint command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.JOINT_DEFINITION
Edit Joint Definition Parameters
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.JOINTMARK
Joint Mark command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.MEASUREMENT_LOCATOR
Measurement Locator command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.NONE
No command.
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.PLUG_SLOT
Plug Slot command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.SURFACE_WELD
Surface Weld command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.USER_DEFINED
User Defined Weld command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.WELD_ATTRIBUTE
Edit Weld Attribute
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.WELD_POINT
Weld Point command
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.WELD_POINT_WIZARD
Weld Point Wizard command
|
Modifier and Type | Method and Description |
---|---|
WeldObjectBuilder.CommandName |
WeldObjectBuilder.commandUsed()
Returns the command name that was last used to create or modify features
License requirements: ugweld ("UG WELD") . |
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static WeldObjectBuilder.CommandName |
WeldObjectBuilder.CommandName.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static WeldObjectBuilder.CommandName[] |
WeldObjectBuilder.CommandName.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.