Package | Description |
---|---|
nxopen.weld |
Provides classes and interfaces for Weld.
|
Modifier and Type | Method and Description |
---|---|
JointmarkGuideBuilder |
JointmarkGuideBuilderList.findItem(int index)
Returns the object at the input index.
|
JointmarkGuideBuilder[] |
JointmarkGuideBuilderList.getContents()
Gets the contents of the entire list
License requirements: None. |
JointmarkGuideBuilder |
JointmarkBuilder.newGuide()
Creates a
JointmarkGuideBuilder object. |
Modifier and Type | Method and Description |
---|---|
void |
JointmarkGuideBuilderList.append(JointmarkGuideBuilder object)
Appends an object to the list
License requirements: None. |
void |
JointmarkGuideBuilderList.append(JointmarkGuideBuilder[] objects)
Appends a set of objects to the list
License requirements: None. |
void |
JointmarkGuideBuilderList.erase(JointmarkGuideBuilder obj)
Erases the object from the list, but does not delete the object.
|
void |
JointmarkGuideBuilderList.erase(JointmarkGuideBuilder obj,
ObjectList.DeleteOption deleteOption)
Erases the object from the list.
|
int |
JointmarkGuideBuilderList.findIndex(JointmarkGuideBuilder obj)
Finds the index where the input object appears.
|
void |
JointmarkGuideBuilderList.insert(int location,
JointmarkGuideBuilder object)
Inserts an object at the specified location
License requirements: None. |
void |
JointmarkGuideBuilderList.setContents(JointmarkGuideBuilder[] objects)
Sets the contents of the entire list.
|
void |
JointmarkGuideBuilderList.swap(JointmarkGuideBuilder object1,
JointmarkGuideBuilder object2)
Exchanges the position of two objects inside the list.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.