public static class WeldPointExitBuilder.FeatureInfo extends Object implements Serializable
Modifier and Type | Field and Description |
---|---|
nxopen.features.Feature |
feature
the newly created or edited feature
|
boolean |
isNewlyCreated
true if a new feature, false if an existing feature was edited.
|
WeldPointExitBuilder.MethodUsed |
methodUsed
the method used to create the feature
|
nxopen.features.Feature |
parent
the parent if method used was mirror or translate
|
Constructor and Description |
---|
FeatureInfo() |
FeatureInfo(nxopen.features.Feature featureInitial,
WeldPointExitBuilder.MethodUsed methodUsedInitial,
nxopen.features.Feature parentInitial,
boolean isNewlyCreatedInitial)
Constructor for the FeatureInfo object.
|
public nxopen.features.Feature feature
public WeldPointExitBuilder.MethodUsed methodUsed
public nxopen.features.Feature parent
public boolean isNewlyCreated
public FeatureInfo()
public FeatureInfo(nxopen.features.Feature featureInitial, WeldPointExitBuilder.MethodUsed methodUsedInitial, nxopen.features.Feature parentInitial, boolean isNewlyCreatedInitial)
featureInitial
- the newly created or edited featuremethodUsedInitial
- the method used to create the featureparentInitial
- the parent if method used was mirror or translateisNewlyCreatedInitial
- true if a new feature, false if an existing feature was edited.Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.