Package | Description |
---|---|
nxopen.uistyler |
PProvides classes and interfaces for User Interface (UI) Styler.
|
Modifier and Type | Field and Description |
---|---|
static FileOperationData.FileOperationState |
FileOperationData.FileOperationState.ENTER
Enter file state
|
static FileOperationData.FileOperationState |
FileOperationData.FileOperationState.EXIT
Exit file state
|
Modifier and Type | Method and Description |
---|---|
FileOperationData.FileOperationState |
FileOperationData.state()
Returns the state
License requirements: None. |
static FileOperationData.FileOperationState |
FileOperationData.FileOperationState.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static FileOperationData.FileOperationState |
FileOperationData.FileOperationState.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static FileOperationData.FileOperationState[] |
FileOperationData.FileOperationState.values()
Returns an array that contains the values for this enum.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.