Package | Description |
---|---|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Field and Description |
---|---|
static ElectricalFormat.Type |
ElectricalFormat.Type.COMPONENTS |
static ElectricalFormat.Type |
ElectricalFormat.Type.CONNECTIONS |
Modifier and Type | Method and Description |
---|---|
ElectricalFormat.Type |
ElectricalFormat.formatType()
Returns the type of
ElectricalFormat
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX5.0.1 |
static ElectricalFormat.Type |
ElectricalFormat.Type.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ElectricalFormat.Type |
ElectricalFormat.Type.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ElectricalFormat.Type[] |
ElectricalFormat.Type.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
ElectricalFormat |
ElectricalFormatCollection.createFormat(String name,
ElectricalFormat.Type type)
Creates a
ElectricalFormat object. |
ElectricalNavigatorFilter |
ElectricalNavigatorFilterCollection.getDisplayFilter(ElectricalFormat.Type type)
Get the displayed
ElectricalNavigatorFilter object
for the given navigator type
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX5.0.1 |
ElectricalFormat |
ElectricalFormatCollection.getDisplayFormat(ElectricalFormat.Type type)
Get the displayed
ElectricalFormat object for the
given navigator type. |
void |
ElectricalNavigatorFilterCollection.setDisplayFilter(ElectricalFormat.Type type,
ElectricalNavigatorFilter filter)
Set the
ElectricalNavigatorFilter object as
displayed filter for given navigator type. |
void |
ElectricalFormatCollection.setDisplayFormat(ElectricalFormat.Type type,
ElectricalFormat format)
Set the
ElectricalFormat object as displayed
format for the given navigator type. |
void |
ElectricalFormat.setFormatType(ElectricalFormat.Type type)
Sets the type of
ElectricalFormat
License requirements: routing_advanced ("Routing Advanced"), routing_base ("Routing Basic") Created in NX5.0.1 |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.