Package | Description |
---|---|
nxopen.routing.electrical |
Provides classes and interfaces for Routing Electrical.
|
Modifier and Type | Field and Description |
---|---|
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.CONNECTOR |
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.DEVICE |
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.NONE |
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.OTHER |
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.SPLICE |
Modifier and Type | Method and Description |
---|---|
ConnectorDevice.ComponentType |
ConnectorDevice.connectorType()
Returns the connector type.
|
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ConnectorDevice.ComponentType |
ConnectorDevice.ComponentType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ConnectorDevice.ComponentType[] |
ConnectorDevice.ComponentType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
ConnectorDevice |
ConnectorDeviceCollection.createConnectorDevice(ConnectorDevice.ComponentType connectorType,
String componentName)
Creates a
ConnectorDevice . |
ConnectorDevice |
ConnectorDeviceCollection.createConnectorDevice(HarnessDevice harnessDevice,
String equipmentName,
String connectorName,
ConnectorDevice.ComponentType connectorType)
Finds or Creates a
ConnectorDevice for given equipmentName and or
connectorName. |
void |
ConnectorDevice.setConnectorType(ConnectorDevice.ComponentType elecRlistComponent)
Sets the connector type.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.