Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static ShipbuildingLinesViewPreferences.ShipbuildingLines |
ShipbuildingLinesViewPreferences.ShipbuildingLines.PLATE
Plate
|
static ShipbuildingLinesViewPreferences.ShipbuildingLines |
ShipbuildingLinesViewPreferences.ShipbuildingLines.PROFILE
Profile
|
Modifier and Type | Method and Description |
---|---|
static ShipbuildingLinesViewPreferences.ShipbuildingLines |
ShipbuildingLinesViewPreferences.ShipbuildingLines.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static ShipbuildingLinesViewPreferences.ShipbuildingLines |
ShipbuildingLinesViewPreferences.ShipbuildingLines.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static ShipbuildingLinesViewPreferences.ShipbuildingLines[] |
ShipbuildingLinesViewPreferences.ShipbuildingLines.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
boolean |
ShipbuildingLinesViewPreferences.getSingleLineRepresentation(ShipbuildingLinesViewPreferences.ShipbuildingLines featureType,
String featureName)
Get single line status
License requirements: None. |
void |
ShipbuildingLinesViewPreferences.setSingleLineRepresentation(ShipbuildingLinesViewPreferences.ShipbuildingLines featureType,
String featureName,
boolean singleLine)
Note: The initial values are set based on the customer defaults depending on
whether the feature is a Profile or a Plate.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.