Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruOptions.layersEdges
Deprecated.
Determines whether edges are displayed for less important
shaded geometry when See-Thru Style is set to Layers.
|
static SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruEdgesType.NORMAL
Deprecated.
Displays edges for less important shaded geometry if edges
are normally displayed for shaded geometry.
|
static SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruEdgesType.OFF
Deprecated.
Displays no edges for less important shaded geometry.
|
SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruOptions.originalColorShellEdges
Deprecated.
Determines whether edges are displayed for less important
shaded geometry when See-Thru Style is set to Original
Color Shell.
|
SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruOptions.shellEdges
Deprecated.
Determines whether edges are displayed for less important
shaded geometry when See-Thru Style is set to Shell.
|
Modifier and Type | Method and Description |
---|---|
static SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruEdgesType.valueOf(int value)
Deprecated.
Returns the enum constant of the specified enum type with the specified value.
|
static SessionVisualizationShade.SeeThruEdgesType |
SessionVisualizationShade.SeeThruEdgesType.valueOf(String name)
Deprecated.
Returns the enum constant of the specified enum type with the specified name.
|
static SessionVisualizationShade.SeeThruEdgesType[] |
SessionVisualizationShade.SeeThruEdgesType.values()
Deprecated.
Returns an array that contains the values for this enum.
|
Constructor and Description |
---|
SeeThruOptions(SessionVisualizationShade.Rgb shellRgbInitial,
SessionVisualizationShade.SeeThruEdgesType shellEdgesInitial,
SessionVisualizationShade.Rgb shellEdgesRgbInitial,
int shellTranslucencyInitial,
SessionVisualizationShade.SeeThruEdgesType originalColorShellEdgesInitial,
SessionVisualizationShade.Rgb originalColorShellEdgesRgbInitial,
int originalColorShellTranslucencyInitial,
SessionVisualizationShade.Rgb layersRgbInitial,
SessionVisualizationShade.SeeThruEdgesType layersEdgesInitial,
SessionVisualizationShade.Rgb layersEdgesRgbInitial,
int layersTranslucencyInitial)
Deprecated.
Constructor for the SeeThruOptions object.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.