Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionSketch.OriginType |
SessionSketch.OriginType.INFER_FROM_PLANE_SELECTION
Sketch origin is inferred from placement face
|
static SessionSketch.OriginType |
SessionSketch.OriginType.PROJECT_WORK_PART_ORIGIN
Sketch origin is the projection of the work part origin
|
Modifier and Type | Method and Description |
---|---|
SessionSketch.OriginType |
SessionSketch.originOption()
Deprecated.
Deprecated in NX8.0.0. Use
SketchInPlaceBuilder.setProjectWorkPartOrigin(boolean) and SketchInPlaceBuilder.setMakeOriginAssociative(boolean) and SketchInPlaceBuilder.setSketchOrigin(nxopen.Point) instead.
|
static SessionSketch.OriginType |
SessionSketch.OriginType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionSketch.OriginType |
SessionSketch.OriginType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionSketch.OriginType[] |
SessionSketch.OriginType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionSketch.setOriginOption(SessionSketch.OriginType originType)
Deprecated.
Deprecated in NX8.0.0. Use
SketchInPlaceBuilder.setProjectWorkPartOrigin(boolean) and SketchInPlaceBuilder.setMakeOriginAssociative(boolean) and SketchInPlaceBuilder.setSketchOrigin(nxopen.Point) instead.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.