Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionPdm.JtUpdateFromSourceType |
SessionPdm.JtUpdateFromSourceType.COMPLETE |
static SessionPdm.JtUpdateFromSourceType |
SessionPdm.JtUpdateFromSourceType.NONE |
Modifier and Type | Method and Description |
---|---|
SessionPdm.JtUpdateFromSourceType |
SessionPdm.jtUpdateFromSource()
Returns the kind of JT update performed when a part is loaded
License requirements: None. |
static SessionPdm.JtUpdateFromSourceType |
SessionPdm.JtUpdateFromSourceType.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionPdm.JtUpdateFromSourceType |
SessionPdm.JtUpdateFromSourceType.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionPdm.JtUpdateFromSourceType[] |
SessionPdm.JtUpdateFromSourceType.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionPdm.setJtUpdateFromSource(SessionPdm.JtUpdateFromSourceType update)
License requirements: None. |
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.