Package | Description |
---|---|
nxopen.preferences |
Provides classes and interfaces for preferences.
|
Modifier and Type | Field and Description |
---|---|
static SessionAssemblies.PositioningTaskCollectionOptionForDesignElements |
SessionAssemblies.PositioningTaskCollectionOptionForDesignElements.CONTEXT |
static SessionAssemblies.PositioningTaskCollectionOptionForDesignElements |
SessionAssemblies.PositioningTaskCollectionOptionForDesignElements.WORK |
Modifier and Type | Method and Description |
---|---|
SessionAssemblies.PositioningTaskCollectionOptionForDesignElements |
SessionAssemblies.positioningTaskCollectionForDesignElements()
Returns the option to specify where to add Design Elements selected whilst working in the Assembly Constraints Dialog.
|
static SessionAssemblies.PositioningTaskCollectionOptionForDesignElements |
SessionAssemblies.PositioningTaskCollectionOptionForDesignElements.valueOf(int value)
Returns the enum constant of the specified enum type with the specified value.
|
static SessionAssemblies.PositioningTaskCollectionOptionForDesignElements |
SessionAssemblies.PositioningTaskCollectionOptionForDesignElements.valueOf(String name)
Returns the enum constant of the specified enum type with the specified name.
|
static SessionAssemblies.PositioningTaskCollectionOptionForDesignElements[] |
SessionAssemblies.PositioningTaskCollectionOptionForDesignElements.values()
Returns an array that contains the values for this enum.
|
Modifier and Type | Method and Description |
---|---|
void |
SessionAssemblies.setPositioningTaskCollectionForDesignElements(SessionAssemblies.PositioningTaskCollectionOptionForDesignElements collection)
Sets the option to specify where to add Design Elements selected whilst working in the Assembly Constraints Dialog.
|
Copyright 2011 Siemens Product Lifecycle Management Software Inc. All Rights Reserved.